Part Number: ISO1452 Other Parts Discussed in Thread: ISO1412 , ISO1450 Can the ISO1452 operate at lower RS485 speeds, like 500 kbps? Any performance concerns with it operating in a 500 kbps system?
We are looking at using it as an alternate to the ISO1412…
Part Number: ISO1452
Hi
I am using the above IC to convert UART data to RS 422 protocol, here i acn transmit data from uart to RS 422 but from RS422 i am unable to receive data,
Part Number: ISO1452 Other Parts Discussed in Thread: ISO1412
Hi TI,
We are facing an issue while using ISO1452 (RS485 and RS422 transceiver) in our custom board. we have a device which works on RS485. here is the command
FF 08 XX XX XX XX 0B (Modified…
Part Number: ISO1452 Other Parts Discussed in Thread: ISO1450 Hi,
Could you let me know if ISO1452 can be utilized for half-duplex as well?
There is ISO1450 supporting half-duplex but customer wants to adopt ISO1452 for both of full-duplex and half-duplex…
Part Number: ISO1452 Hello.
I'm interested at what cable length is it possible to achieve a throughput of 50Mbps with ISO1452. I didn't find any information in datasheet? there are only general curves with maximum 10Mbps curve.
Thank you.
Andriy…
Part Number: ISO1540 Other Parts Discussed in Thread: ISO1452 , ISO1450 Hello team,
Is it possible to use those ISO154x bidirectional I2C isolators for isolating other communication protocols which are not I2C ?
Specifically I thought to use it for isolating…
Hi Ade,
Sorry, I shared ISOW1432 because that is what in the title of this E2E post but I understand that you are planning to use ISO1432 for your application. Since ISO1412, ISO1432 and ISO1452 are all pin-compatible, we have one common EVM ISO1412DWEVM…
Hi Nandha,
Thanks for sharing the schematic for review.
The schematic looks good and i do not see any major concerns. Please make sure you follow the PCB layout guidelines from datasheet.
For isolated power supply solution, we also have SN6505B / SN6505A…
Part Number: ISO35 Other Parts Discussed in Thread: ISO1412 Team,
The ISO35DWR is being used in a project. Looking at the product page different ISO14xx/ISO15xx/ISO30xx might be used as P2P alternative: ISO1412 vs ISO1432 vs ISO1452 vs ISO35 vs ISO3080…
Part Number: AM26LV32 Other Parts Discussed in Thread: AM26LV31 , ISO1452 , ISO1450 , ISO7760 Hi team,
We are currently using single-ended differential level conversion chips AM26LV32 and AM26LV31. Is there an isolated type? The requirement is that the delay…