Part Number: ISO1640 Dear TI Experts,
According to datasheet of ISO1640BD:
Same side ±8 kV IEC-ESD unpowered contact discharge on SCL2 and SDA2 (Side 2)
I am wondering whether it is possible to get the same electrical characteristic but when…
Part Number: ISO1640 Hi Team,
We were planning to use ISO1640 part for Bi-directional open drain GPIO signals.
I would like to simulate the device functionality using simulation.
Request you to share the simulation model for ISO1640.
Regards,
D.Meenalochini…
Part Number: ISO1640-Q1 Other Parts Discussed in Thread: ISO7721-Q1 , ISO6721-Q1 , , ISO6721 , ISO7721 , ISO1640 Hello team,
My customer is looking for UART isolator.
I cannot recommend digital isolator such as ISO6721-Q1, ISO7721-Q1 because customer wants…
Part Number: ISO1640-Q1 Other Parts Discussed in Thread: ISO1640 We are looking to replace the SI8600, we have used the SI8600AC-B-ISR.
We need,
Minimum Isolation Voltage: 1500Vrms
Minimum Creepage: 2.9mm
Minimum Clearance: 2.3mm
Must have a UL certi…
Part Number: ISO1640 Good morning We are using I2c Isolator ISO1640. To simplify the PCB we have connected, in input, the SDA signal on pin 3 (SCL1) and the SCL signal on pin 2 (SDA1).
Outgoing the same thing.
Is this possible or must the SDA and SCL signals…
Part Number: ISO1640 Other Parts Discussed in Thread: ISO1540 Hi Sir,
may we know and learn from you, why does side1 have this low to high transition? thanks.
Part Number: ISO1640 Other Parts Discussed in Thread: ADS112C04 Hello TI's isolation parts expert team,
I am evaluating ISO1640 and ADS112C04 and try to use ADS112C04 in isolated condition by ISO1640.
However, when I insert ISO1640 between microprocessor…
Part Number: ISO1640 Other Parts Discussed in Thread: ISO1644 , Hi Team,
We would like to ask your help regarding the customer's inquiry below.
VDE certification I have seen in the web ti page of the product ( www.ti.com/.../ISO1640 certification VDE…
Part Number: ISO1640 Other Parts Discussed in Thread: ISO7741 Hi Team,
My customer need CAD drawing of the SOIC(DW) package. It is not released on the website. When do we have RTM of the package version? I saw we only have pre-production samples online…