Part Number: ISO224 Other Parts Discussed in Thread: AMC3330 Hi Team,
My customer planning to accurately measure bi-directional voltage from ISO224 chip in a 3 phase AC motor controller application.
In their application , the motor will be connected…
Hi Kai,
The pulse width is 10us, I think output signal of ISO224 has 2-3 us delay is normal. the LM6132 OUTA has delay but still around 10 us, just not understand why OUTB pulse width is shorter.
Measure output signal of ISO224 needs differential probe,…
Part Number: ISO224 Other Parts Discussed in Thread: TINA-TI I needed ISO224 generic model PSPICE file for analysis in one of our project. If anyone can help with that it will be really helpful.
Part Number: ISO224 Other Parts Discussed in Thread: AMC1302 , AMC1300 , AMC3302 , AMC3301 , INA149 , AMC1336 , AMC3330 , AMC1350 , AMC1351 ..
Hi,
I am not able to find common mode voltage range for ISO224 in the datasheet. I want to use it for 900V System as…
Part Number: ISO224 We use ISO224 to measure HV voltage AC/DC power converter.
We calibrated the measurement circuit with low noise voltage source and the accuracy is very acceptable. But when we connect the measurement circuit to noisy circuit like DC…
Part Number: ISO224 I am currently working a PCB layout using the ISO224BDWVR isolation amplifiers. I am looking at the recommended layout example on the datasheet (section 11.2) particularly the clearance area that is to be kept free of any conductive…
Part Number: ISO224 Other Parts Discussed in Thread: AMC3330-Q1 Hello,
Please confirm if ISO224 has Automotive application qualification/certification. Refer me to alternate solution with Auto certification part considering similar specification.
Thanks…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: ISO224
Hi Team,
"Error(ORPSIM-16103):Invalid value" occurs when I try to do AC analysis for ISO224.
I looked up this error code online and someone says this error causes by setting…