tens of MCUs have been replaced.
The thing is when I replace MCUs the problem always moves with the problematic part.
The interface device is TI ISO35T connected directly to the MCU UART.
I've the
MSP-TS430PN80USB - 80-pin Target Development Board…
Other Parts Discussed in Thread: ISO35T Hi,
My customer will use ISO35T.
If there is a transformer of recommendation, please tell me.
(Something of a surface mounting-type is desirable)
Best regards, itabi
Other Parts Discussed in Thread: ISO35T Hi
The VDE 4001631 and UL E181974 of ISO35T are written as pending in datasheet, but are these authorized already?
Regards, PAN-M
Other Parts Discussed in Thread: ISO35T Dear all.
Please teach me about the isolation voltage of the ISO35T. 1) The design limitation of isolation voltage and impressing time. (RMS/Peak) 2) The guarantee of isolation voltage and impressing time. (RMS/Peak…
Other Parts Discussed in Thread: ISO35T , ISO35 Hello, Could you please let me know the connection of unused D1,D2 pin of ISO35T ? Can we float these pins?
Best Regards, Ryuji
Other Parts Discussed in Thread: ISO35T Hello!
For my application, I'll use the ISO35T.
I found it is only available as SMD. Is it avaliable as Through-hole Package as well ?
or, why is this transceiver just as SMD?
It is just, that soldering by h…
Other Parts Discussed in Thread: ISO3086T , ISO35T Hello, all
Now we have one inquiry from our customer who is considering to use ISO3086T or ISO35T.
They have fixed the VCC1 input voltage to 3.3V, however has not fixed the VCC2 input voltage on either…
Other Parts Discussed in Thread: ISO35T Dear all,
I am experiencing a high death of the ISO35T driver line. I use the ISO35T in half duplex mode with the pin Y connected to a with a 10K pull-up (3.3V) and the pin B connected to Z with a 10K pull-down…
Hi Jared,
I would like to use wkup_uart0 for debug console in j784s4-evm board and I was able to do that using board-support packages. in this process I bypassed OPTEE image inclusion in BL31 using below command.
make CROSS_COMPILE=/home/sandra/ti/arm…