Part Number: ISO5852S
Hi,
I am planning to build a two-stage inductive adder with each layer operating below 700 V. I am planning to use a SiC MOSFET which is a low-side FET in inductive adder configuration. Can I use ISO5852S to drive the FET in this…
Part Number: ISO5852S Other Parts Discussed in Thread: UCC21732 Hello,
As per the ISO5852S datasheet (SLLSEQ0B –AUGUST 2015–REVISED JANUARY 2017) section 9.4 Device Functional Modes Table 1 (function table), the driver output is held low when IN- is High…
Part Number: ISO5852S Hi,
The datasheet states that the maximum isolation voltage rating of ISO5852S is 5.7 kV. However, some literature proposes custom gate driver design for 10-15 kV MOSFET module using this IC. From my understanding, the technique…
Part Number: ISO5852S Hi Team,
I have a question regarding the PCB layout of the gate driver IC ISO5852S. This IC has 2 VEE2 pins, one on the top and the other on the bottom. Should both of them be connected, or one of them is enough?
Beat Regards, Tom…
Part Number: ISO5852S-Q1 Hi Team,
I am working with ISO5852S-Q1 for Drive Development.
From DSP through Buffer IC the PWM are transferred to the gate driver.
I have these observations
1) If am connecting my laptop charger and JTAG together with low…
Part Number: ISO5852S Hi team i'm looking for a driver wich can detect Short circuit or another fault signal of Si or SiC Fets. İs it possible with ISO5852S? or is this only for IGBT. Best Regards.
Part Number: ISO5852S Hi Team, May I ask for your confirmation and expertise? My customer is designing a driver PCB for 4.5KV IGBT, IC based, He used ISO5852 for 1700V IGBT.
Can he use ISO5852 for 4.5KV IGBT Gate driver with external buffer? We will wait…
Part Number: ISO5852S Other Parts Discussed in Thread: TIDA-01606 , Dear all,
I am trying to create a system to test the gate driver cards E2 which are used on the TIDA-01606 power converter design.
I am having difficulties understanding how the DESAT function…
Part Number: ISO5852S-Q1 Other Parts Discussed in Thread: ISO5852S InsulationCoordination_HVInverter_19052021.pdf
Hello,
We're designing Automotive motor drive with UDC MAX = 880V. Regarding standard we need creepage min. 10mm. All your reinforced isolated…
Part Number: ISO5852S Hi, Good day. Our customer wants to know what to do with the DESAT if they not going to use its functionality. Looking forward to your inputs. Regards, Cedrick