Part Number: ISO5852S-EP Other Parts Discussed in Thread: ISO5852S we are using a schottky diode ( NRVBAF3200T3G) across desat pin to limit the negative voltage spikes. As per the ISO5852S datasheet this pin will withstand up to -0.3V. as per the selected…
Part Number: ISO5852S-EP Other Parts Discussed in Thread: UCC21750 Hi Team,
We are using the part number ISO5852-EP. Followings are the technical question for the same part.
1. As per data sheet (VIT+UVLO) is typ-12V , Max-13V and (VIT-UVLO) is typ-9…
Part Number: ISO5852S-EP Other Parts Discussed in Thread: ISO5852S
Hi Team,
Hope you are doing good.
I am using ISO5852S in my 3 phase inverter application, In short circuit or Over current condition plannig to shutdown all the 06 IC's together. For that…
Part Number: ISO5852S-EP Hi,
The basic calculations in Table A7.1 of AEC-Q100 (reproduced in figure) for each of the major stress components, demonstrate how one can derive the reliability margin between the component (specification) space and the application…
Part Number: ISO5852S-EP
Hi All,
I am using ISO5852 isolated gate driver in my inverter application. In that I have connected all the Fault signals together with a common pull up resistor to VCC. In internal circuit diagram of IC FLT pin is directly…
Part Number: ISO5852S-EP Hi Team,
Hope you are doing well,
I am Vivek Gandham, I am using the mentioned 06 Isolated gate drivers in my application. In this Gate driver Ready and Fault signals are given to GPIO's, Due to less GPIO's in my processor, I…
Part Number: ISO5852S-EP Other Parts Discussed in Thread: ISO5852S
[reposted due to photo display issue]
Hi TI representatives,
We are using ISO5852s for half-bridge SiC MOSFET. VDC bus is ~200V and target to trigger DSAT at Vds ~ 1.4V in less than 2…