Part Number: ISO6721-Q1 Tool/software: Dear all,
is the Tj,max<150°C condition (in the abs.max. section of the datasheet) enough to guarantee that the ISO6721-Q1 works in safe conditions, no matter what Ta we have?
Thank you very much in advance …
Part Number: ISO6721-Q1 Hello guys,
One of my customers is considering using ISO6721-Q1 for for level shifting from 2V to 3.3V with isolation.
At this moment, they have the following questions? Could you please give me your reply?
Q1. Can ISO6721…
Part Number: ISO6721 Other Parts Discussed in Thread: , ISOW7721 Hello All,
I want to use ISO6721 as a Digital UART Isolator. Currently my hardware is USB Powered & I'm using a 5V to 3.3V LDO (TPS73633) to use 3.3v for MCU and other IC's on PCB.
I…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: MSP-FET , ISOUSB211
Tool/software:
Hi. There is something related to galvanic isolation which I am confused about. It is not actually related to ISO6721-Q1, it involves microcontrollers and…
Part Number: ISO6721 Other Parts Discussed in Thread: ISOUSB211 , ISOUSB111 Tool/software: I want to isolate the communication of the USB serial port. Can the digital isolator be used for USB isolation? Can this solution be implemented through peripheral…
Part Number: ISO6721 Hello All,
I'm trying to use ISO6721 as digital UART isolator between my MCU and CP2102 .
I wanted to know about the TX, RX connections between the IC's.
MCU TX to ISO6721 pin No. 2 (OUTA)
MCU RX to ISO6721 pin No. 2 (INB…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: ISO6721 Tool/software: HI team,
I have a project and plan to use the ISO6721 for isolated UART communication.
When system is low power mode there is no communication through ISO6721. The Low…