Part Number: ISO6721-Q1 Tool/software: Dear all,
is the Tj,max<150°C condition (in the abs.max. section of the datasheet) enough to guarantee that the ISO6721-Q1 works in safe conditions, no matter what Ta we have?
Thank you very much in adva…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: ISO6721 , Tool/software: Hello
Thank you for reading this message.
I am doing an isolated RS232 serial communication, for this I am using the ISO6721RBQDRQ1 connected as shown in the image, the signals…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: ISO6721 Tool/software: Hi TI Teams
Schematic Prints.pdf
We use ISO6721 between High and Low voltage side MCU(TI MSPM0G3507SR) uart port,and sometims the uart abnormal.
If we want to add a RC filter…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: ISO7721-Q1 , , ISO7721 , ISO7710 Hi
what is the frequency of
ISO7721-Q1 and
ISO6721-Q1
internal oscillators ? (i.e. oscillator block according to the datasheet)
Do they use any kind of spread spectrum…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: ISO6721 Tool/software: HI team,
I have a project and plan to use the ISO6721 for isolated UART communication.
When system is low power mode there is no communication through ISO6721. The Low voltage…
Part Number: ISO6721-Q1 Other Parts Discussed in Thread: ISO6721 , ISO6741 Hi team,
As we know,ISO7221 is TTL input type and ISO6721 is CMOS input type. Do you have any suggestion on the compatible design on these two device?
ISO6721 input voltage:
ISO7221…
Part Number: ISO6721-Q1 Hello guys,
One of my customers is considering using ISO6721-Q1 for for level shifting from 2V to 3.3V with isolation.
At this moment, they have the following questions? Could you please give me your reply?
Q1. Can ISO6721-Q1 be used…
Part Number: ISO6721-Q1
Hi, Support Team
We use ISO6721-Q1. INB pin connected to GND, When power on and we find OUTB have peak voltage 2.92V
is normal?
note: OUTB Pin is floating
Schematic:
SCOPE:
if any suggestion, Please advise me.
Thanks,
Best regards…
Part Number: ISO6721-Q1 Hi Team,
Can you please help with diagnosing the issue with the IBIS model of ISO6721FQDWVRQ1? Please see error below:
Thanks in advance.
Regards,
Marvin
Part Number: ISO6721-Q1 Hi Expert,
Customer is using ISO7721QDRQ1 for mass production. Now we are using ISO6721BQDRQ1 to replace ISO7721QDRQ1 due to supply issue. Could you share the difference between those two devices?
Because end car OEM need this information…