Part Number: ISO6731 Hi Good Afternoon Can you suggest the, digital Isolators, part number for the below requirements mentioned
Isolation Resistance
10M Ohms @ applied voltage of 1000V
-Degree of Contamination
Class II as per IEC 60664-1
-Over…
Part Number: ISO6731 Hi,
The power supply voltage range in the ISO6731FDWR manual is 1.71V to 1.89V and 2.25V to 5.5V, as shown in the following figure. May I ask if the voltage devices in the range of 1.89 to 2.25 cannot work? Why?
Thanks!
Part Number: ISO6731 Hi Team,
I have a question of Supply voltage range as its in the datasheet below:
Why the recommend VCC range is not Continuous like 1.71~5.5V?
Are there any problems if my customer use 1.9V for VCC?
BR,
Moon
Part Number: ISO6731 Hello,
I admire your isolators, for example iso6731.
You offer two version of the "default output": High or Low (F suffix).
So you need to manufacture double the number of models,
distributors need to keep double space…
Part Number: ISO6731 Dear Specialists,
My customer is considering ISO6731 and has a question.
I would be grateful if you could advise.
---
Is ISO6731DWR Basic Isolation or Reinforced Isolation.
---
I appreciate your great help in advance.
Best regards…
Part Number: ISO6731-Q1 Other Parts Discussed in Thread: TMS320F280037C I am using this type of isolator having signal DSP_CAN_RX and DSP_CAN_TX , which is connected to TMS320F280037C controller. I want to know the
…
Part Number: ISO6731 Other Parts Discussed in Thread: ISO7731 , , , ISO7731-Q1 , ISO7831 , ISO7331-Q1 , ISO7741 , ISO7742 Hi Team,
Our customer is in dire need of ISO6731 or an alternative for this device. I looked at our products list and the drop-in repla…
Part Number: ISO6731 Other Parts Discussed in Thread: ISO7731 The datasheet for ISO6731 states a tPZH delay of max. 23ns, whereas the ISO7731 datasheet shows a tPZH delay of max. 8.5us for the F-version under Vcc=3.3V conditions. This is 100 times more…
Hello,
Thank you for your question.
The ISO7710 device has no EN pin, as shown in the datasheet: ISO7710 High Speed, Robust EMC Reinforced Single-Channel Digital Isolator datasheet . Please see image below:
If you require a EN pin for the isolator device…
Other Parts Discussed in Thread: ISO6731 We have use SN75176AD in our product but, observed same issue.
1) main micro controller and PC communication issue.
Refer attached design and suggest correct solution.