Part Number: ISO6740 Other Parts Discussed in Thread: STRIKE Hi team,
Could you help me to clarify the ESD specification of ISO6740?
I'd like to clarify the bias condition of each pins under the HBM and CDM tests.
In HBM and CDM, it is described…
Part Number: ISO6740 Other Parts Discussed in Thread: ISO7740 , ISO7740-Q1 , Hi
Please help with si8640 comparison difference table
Si864x Data Sheet (mouser.tw)
Part Number: ISO6740-Q1 Other Parts Discussed in Thread: ISO1212 Hi Team,
Our customer is looking for a 4-channel automotive isolator to determine if a 12V/24V signal is on or off.
For example:
- If the break light of the car is on, the voltage…
Part Number: ISO6740 Hi team,
I received a question from the customer.
The customer is concerned about min time of propagation delay time at 5-V supply.
I understand that only Typ and Max are defined.
From the PWD, If L->H tPLH is 18 ns (max)…
Part Number: ISO6740-Q1
ISO6740QDWRQ1 is used in our design as shown below, the sense signals(INx and OUTx) are of 5V level and VCC=3.3V. According to the datasheet INx and OUTx maximum voltage rating is VCCx+0.5, but we wanted to know if INx and OUTx…
Part Number: ISO6740 Hi team,
Could you give me comment on following customer questions?
Q1. When the customer doesn't use 2 ch out of 4 ch, the supply current - ac signal is proportional to the number of using channel. is it correct understanding…
Part Number: ISO6740-Q1 Other Parts Discussed in Thread: ISO6740 , ISO7741 , ISO7710 Hi,
I am searching for an digital isolator where i can tristate outputs whenever required from the input side. ISO6740-Q1 has enable EN2. Is EN2 referenced to VCC2…
Part Number: ISO7840 Other Parts Discussed in Thread: UCC27714 , ISO7740 , ISO6740 , Tool/software: The OUT signal of the ISO7840F occasionally becomes unstable. When VCC1 = 3.3V, VCC2 = 5V, EN2 = 5V, and INA = 0V (Low), OUTA is output at a fixed 2.5V…
Part Number: ISO6540 Other Parts Discussed in Thread: TXG4041 , , ISO6740 , ISO7740 , ISO6441 Tool/software: I need voltage level translation product that also provides 12V of isolation between the A and B sides of the IC. Currently looking at the ISO6540…
Part Number: ISO7340C Other Parts Discussed in Thread: ISO7230C , , ISO6740 Tool/software: Dear Specialists,
My customer is considering ISO7230C and has a question.
I would be grateful if you could advise.
---
According to HP Certifications and…