Part Number: ISO6740-Q1 Tool/software: If the VCCx, specifically VCC1 is 5V, then can the INx be of 5V level and perform translation to 3.3V out with VCC2 as 3.3V?
Part Number: ISO6740-Q1 Tool/software: Hi team,
Can the ISO6740-Q1 be used with VCC1 side at 1.8V and VCC2 side at 5V, since there are two sets of operating voltages
Thanks,
Pream
Part Number: ISO6740-Q1 Other Parts Discussed in Thread: ISO1212 Hi Team,
Our customer is looking for a 4-channel automotive isolator to determine if a 12V/24V signal is on or off.
For example:
- If the break light of the car is on, the voltage…
Part Number: ISO6740-Q1
ISO6740QDWRQ1 is used in our design as shown below, the sense signals(INx and OUTx) are of 5V level and VCC=3.3V. According to the datasheet INx and OUTx maximum voltage rating is VCCx+0.5, but we wanted to know if INx and OUTx…
Part Number: ISO6740-Q1 Other Parts Discussed in Thread: ISO6740 , ISO7741 , ISO7710 Hi,
I am searching for an digital isolator where i can tristate outputs whenever required from the input side. ISO6740-Q1 has enable EN2. Is EN2 referenced to VCC2…
Hello Gareth,
Unfortunately, we do not provide competitor comparison tables on this forum. All the information needed to compare ISO6740 can be found on the product page ( ISO6740 data sheet, product information and support | TI.com ) and corresponding…
Part Number: ISO7340-Q1 Other Parts Discussed in Thread: ISO7740 , ISO6740 Hi, Good day. Our customer wants to use the ISO7340FCQDWQ1 but they cannot find the Insulation Lifetime Projection Data for this device. Can you pleas help us provide the curve…
Part Number: ISO6740 Hi team,
Could you give me comment on following customer questions?
Q1. When the customer doesn't use 2 ch out of 4 ch, the supply current - ac signal is proportional to the number of using channel. is it correct understanding…
Part Number: ISO6762 Hello,
we were wondering, why the ISO6762 is neither listed in the UL File No. FPPT8.E181974, nor in the UL-CA-L181974-24-32205102-8, even though it is mentioned under "PRODUCTs COVERED" in "USR/CNR - Single Protection, Non-Optical…
Hi Tom,
Please see attached the updated UL certificate. It lists ISOM8111 (DFS package) at 5000 Vrms.
I'll be posting this certificate online within the next month.
Thanks, Saleem Marwat
UL Certificate of Compliance File E181974 Vol 4 Sec 6.p…