Part Number: ISO6741 Other Parts Discussed in Thread: ISO7841 , ISO7741 Similar question for the ISO6741. Can you please let me know if the carrier frequency is the same for ISO6741 (450MHz).
Thank you, Oliver
Part Number: ISO6741 Hello,
I see in the datasheet that this part is rated UL for single isolation. Do you plan to have the reinforced isolation also? Do you have something in your catalogue that is reinforced isolation ready?
Thank you,
Mattia Berto…
Part Number: ISO6741 Hello, I have a question for VCC1/2 range of ISO6741.
According to the datasheet, both VCC1 and VCC2 has two different ranges, 1.71-1.89V and 2.25-5.5V. Does it mean it doesn't support 1.89V-2.25V range? Why don't you specify simply…
Part Number: ISO6740 Other Parts Discussed in Thread: ISO6760 , , ISO6741
Hi team,
My customer would like to know the VCCI threshold voltage to output default for ISO6740, ISO6741, and ISO6760.
Which one my customer should follow?
1. VCC<=1.05V described…
Part Number: ISO6741 Hello, According to the datasheet, all safety-related certifications are "planned". When will you get each certification? Will you get all certifications when you start the production?
Regards, Oba
Hi, thanks for your reply, regarding response 1 and 2, I have some questions below:
1. It means that the Auto pin can be left open?
2. (1) Reasons why ISO7241 is not recommended?
(2) Can ISO7241 and ISO6741 be pin to pin?
Thanks Jalen,
Hi Pete,
Thanks for reaching out. As Clemens stated, please do check if your application requires isolation. If isolation is required, then you can isolate power and signals using various isolation devices but this doesn't reduce any cabling…
Hi Kaveh,
Thank you for reaching out.
It is common to use isolators to isolate a gate drive signal to switching components. Please find below my suggestions, thanks.
If you already have a gate driver to drive SiC FETs, then you can use digital isolators…
Part Number: SN65HVD485E Other Parts Discussed in Thread: ISO3082 , ISO1432 , ISO6741 , ISO7741 , ISO6721 , ISO7721 Hi,
I am working on an RS-485 interface design. I am looking for a digital isolator that is compatible with the Tx and Rx pins of the SN65HVD485E…