Part Number: ISO6760 Dear TI team,
I am using ISO6760DWR as digital isolator in my circuit. Input side Vcc is 3.3 V but input PWM signal is 5 V.
Vi is higher than Vcci but it is below absolute maximum rating. Will this configuration damage my circuit…
Part Number: ISO6760 Dear TI team,
I am using ISO6760DWR as digital isolator in my circuit. I am observing that voltage at the OUT pin of IC ISO6760DWR is continuously high.
Note that, I have not connected pull down resistor at the input and input…
Part Number: ISO6760 Other Parts Discussed in Thread: ISO6763 Hi Team, I want to isolate the SPI signal from a Printed Circuit Broad while entering another Printed Circuit Broad. So I choose the isolator ISO6760. The SPI from the main board is a 1.8V…
Part Number: ISO6760 Other Parts Discussed in Thread: ISO7762DWEVM , ISO7760 , ISO7762 Hi TI,
Could you please help me find a replacement for ISO6760FDWR with the same pinout and same package/case.
I have used this in my design and now it is out of…
Part Number: ISO6760 Hi team,
Customer implements RC filter at ISO6760 input. The value is R = 600ohm, C = 330pF.
Do you have recommended range for each value? Are there any effect by increasing resistor value?
Best regards,
Hayashi
Part Number: ISO6760-Q1 Hi expert,
I want to confirm that when VCCO is in PD state, is it possible to pull the output string resistor low to GND to achieve the default state as low? If not, do you have any suggestion?
Part Number: ISO6760-Q1
I am using device - ISO6760QDWRQ1 and wanted to know the supply currents (ICC1 & ICC2) when my VCC1=5V and VCC2=3.3V. I have considered below supply currents as maximum possible supply currents.
Is my understanding correct…
Part Number: ISO6760 Hi team,
I would like to ask the device VIH and VIL.
1. Since VIH (min) = 0.7*Vcc, VIL (max) = 0.3*Vcc, VIT+ (max) must be same as VIH (min), VIT- (min) must be same VIL (max). It is obviously, but are all tested?
2. If tested…
Part Number: ISO6760 Dear team,
When I read datasheet of ios6760, I figured out our datasheet showed two different Vcc1 on line 1 and line2. Same as VCC2 on line 3 and 4. Can you help explain why? Thanks!
Part Number: ISO6740 Other Parts Discussed in Thread: ISO6760 , , ISO6741
Hi team,
My customer would like to know the VCCI threshold voltage to output default for ISO6740, ISO6741, and ISO6760.
Which one my customer should follow?
1. VCC<=1…