Part Number: ISO6761 Other Parts Discussed in Thread: ISO6461 , ISO6421 Hi,
Is it possible to use ISO6761 as a SPI isolator to interface between a sensor which operates at 1.8V and a MCU (Apollo blue 4) which operates at 2.2V SPI ?
Are there any alternative…
Part Number: ISO6761-Q1 Tool/software: Hi Team,
I have 3V3_Standby supply which comes before P3V3.
Both are referenced to same digital ground.
1. Is there any sequence requirement? Can VCC1 alone be powered till VCC2 is up?
2. can IN pins be…
Part Number: ISO6761 Hi We are using this ISO6761DWR one of our product. ,
We are using one more programmer device in parallel (either one connect at a time),
Other programmer used from IAR I-JET programmer , This is Always high state in normal. …
Part Number: ISO6761 The datasheet reports the creepage and clearance values (CLR and CPG, pg.8) are >8mm but the suggested footprint shows copper that is <8mm apart between the isolated pins. What is the recommended footprint layout to maintain >8mm…
Part Number: ISO6761 Other Parts Discussed in Thread: SN6501 , ISO6762 I check the isolation of my complete board by applying 750VDC across the isolated regions.
Often I'm finding the IS6761 being damaged after this test.
This doesn't always happen…
Part Number: ISO7761 Other Parts Discussed in Thread: ISO6761 Hi team,
ISO7761 does not support 1.8V. Is there any similar device that can support 1.8V?
BR,
Comi
Part Number: AMC131M03 Other Parts Discussed in Thread: ADS131M04 , , SN74LVC1G17 , AMC3336 , AMC1336 , AMC0386 , SN6501 , UCC33020 , ADS1204 , ISO6761 Tool/software:
Hi im using AMC131M03 and ADS131M04, im having an issue in crc, in what are the ways…
Part Number: ISO6760L Other Parts Discussed in Thread: ISO6761-Q1 , ISO6762 Hi Team,
Can you please provide the IBIS model for the following parts?
ISO6760L ISO6761-Q1 ISO6762
I hope you can help.
Regards,
Marvin
Part Number: ISO6741-Q1 Other Parts Discussed in Thread: ISO6760-Q1 , ISO7741-Q1 , ISO7760-Q1 , ISO7761-Q1 , ISO6761-Q1 Hi Im looking for alternate part for ISO6741-Q1 with 5/0, 5/1 , 6/0 or more channels Isolator. I need enable control on output. Please…