Part Number: ISO7021 Please provide the latest updated CMRT for the following parts, thank you.
ATL431LIBQDQNR
TPS7B8401QWDRBRQ1
ISO7021DR
TPS22810DBVR
Part Number: ISO7021 Hi,
I would like to confirm whether the ISO7021 isolator can be used for isolation from a 3.3V logic side to another 3.3V logic side. The PWM signal frequency is 100 kHz, and it is generated from the TMS320F28379DPTPS.
If this…
Part Number: ISO7021
Tool/software:
Hi,
I have a question regarding ISO7021 and ISO7021F outputs.
ISO7021 (without suffix F) - default output is High.
ISO7021F (with suffix F) - default output is Low.
In the datasheet, the switching characteristics…
Part Number: ISO7021 Tool/software: Hi All,
A customer is considering switching from photocouplers to ISO7021.
Could you please let me know if there is a way to compare and evaluate the noise immunity performance of photocouplers and ISO7021?
What…
Part Number: ISO7021 I am currently having an issue with our notified body for Ex marking of a product where we use ISO7021 for IS-IS separation. They state that the device itself has to be marked with IECEx and ATEx in order for them to accept is as…
Part Number: ISO7021 Hi All,
I have a question regarding Supply Current.
1) I understand each Supply Current as below, is it correct?
2) Supply current - Please tell me how to calculate the current value for each transmission rate of AC…
Part Number: ISO7021 I have a question regarding the supply voltages for the ISO7021.
My application requires VCC1 to equal 2.50V. I would like VCC2 to be adjustable from 1.8V to 3.3V.
What range of voltage can VCC2 be? Is it limited to 2.25V to 5…
Part Number: ISO7021 In the SLLSFAOB application note in section:
9.1.2 Intrinsic Safety The ISO7021 supports Intrinsically Safe (IS) to IS applications and carry IECEx and ATEX certifications. These devices do not currently support IS to non-IS galvanic…
Part Number: ISO7021 Based on the SLLSFAOB application note the ISO7021 completed the validation and test.
9.1.2 Intrinsic Safety The ISO7021 supports Intrinsically Safe (IS) to IS applications and carry IECEx and ATEX certifications. These devices…
Part Number: ISO7021 The datasheet recommend operating conditions suggest that if one side is at 1.8V supply, then the other side can only be between 1.71 -> 1.89V.
Does this mean that it will not work with a 1.8V supply and a 3.3V supply, or am I misunderstanding…