Part Number: ISO7021
Tool/software:
Hi,
I have a question regarding ISO7021 and ISO7021F outputs.
ISO7021 (without suffix F) - default output is High.
ISO7021F (with suffix F) - default output is Low.
In the datasheet, the switching characteristics are…
Hi Ishiwata-san,
Shuji Ishiwata said: For example, what frequency noise can be eliminated? Also, what voltage level noise can be eliminated? This is information that customers would like to know.
This information is primarily found in the datasheet itself…
Part Number: ISO7021 I have a question regarding the supply voltages for the ISO7021.
My application requires VCC1 to equal 2.50V. I would like VCC2 to be adjustable from 1.8V to 3.3V.
What range of voltage can VCC2 be? Is it limited to 2.25V to 5.5V…
Part Number: ISO7021 Hi All,
I have a question regarding Supply Current.
1) I understand each Supply Current as below, is it correct?
2) Supply current - Please tell me how to calculate the current value for each transmission rate of AC.
Best Regards…
Part Number: ISO7021 The datasheet recommend operating conditions suggest that if one side is at 1.8V supply, then the other side can only be between 1.71 -> 1.89V.
Does this mean that it will not work with a 1.8V supply and a 3.3V supply, or am I…
Part Number: ISO7021 In the SLLSFAOB application note in section:
9.1.2 Intrinsic Safety The ISO7021 supports Intrinsically Safe (IS) to IS applications and carry IECEx and ATEX certifications. These devices do not currently support IS to non-IS galvanic…
Part Number: ISO7021 Based on the SLLSFAOB application note the ISO7021 completed the validation and test.
9.1.2 Intrinsic Safety The ISO7021 supports Intrinsically Safe (IS) to IS applications and carry IECEx and ATEX certifications. These devices do…
Part Number: ISO7021 Hello,
I would like to use ISO7021 to isolate MSP432 Launchpad debug interface. MSP432 works 1.8-3.6V. In ISO7021 datasheet there is two voltage range around 1.8V and 2.25-5V. Does it mean I can not use it continuously in the MSP…
Part Number: ISO7021
Hi ,
need to understand device behavior when ISO get a very low frequency signal on the input that need to be acquired promptly. If the input is stable for more than 100ms and an impulsion is applied on the input does this information…