Part Number: ISO7241C-Q1 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hi Team,
Looks like there is only IBIS model available for this part. One of my customer is requesting for PSPICE model. Do we have one available for…
Part Number: ISO7241C Other Parts Discussed in Thread: TPS2388 , ISO7341FC Hi,
I am designing my circuit with ISO7241C. I want pass OSS signal from external MCU to TPS2388 device and the OSS pin is internally pulled down to GND. When I use ISO7241 to pass…
Other Parts Discussed in Thread: ISO7241C Hello,
Our customer use the ISO7241C, have a latch-up issue.
The customer check the system level protection of ESD .
The system level standard is the IEC61000-4-2.
Before discharge to EUT, the customer discharge…
Other Parts Discussed in Thread: ISO7241C Do we have any data on the typical output rise and fall specification? Do we have a histogram that I could share with the customer?
Thanks for your help with this!
Richard Elmquist
Hamamoto -san,
1.5 times is good estimate for the max currents to typical ratio even at 2Mbps. The 1Mbps to 2Mbps dynamic current contributions are quiet similar.
Regards,
Sarangan Valavan
Other Parts Discussed in Thread: ISO7641FC , ISO7241C , DAC161S997 , ISO7841 Objective: To interface DAC161S997 , with Microcontroller C8051F350 through ISO7641FC using SPI Protocol, Which works fine and DAC output is achievable.
Now here is the problem, I have…
Other Parts Discussed in Thread: ISO7241C What is the typical supply current of the ISO7241C when both enable lines are low, Vcc1 is at 0V, and Vcc2 line is connected to a 5V supply?
Other Parts Discussed in Thread: ISO7241C I have a customer asking the question below:
TI ISO7241C part -
The data sheet states that the part “operates with 3.3V or 5V“. The “Recommend Operation Conditions” table has a note that states:…