Part Number: ISO7341-Q1 Other Parts Discussed in Thread: ISO6741-Q1 We have built some boards using the ISO7341CQDWQ1 chip. Due to an error, the bypass caps are 1.0uF instead of the 0.1uF in the data sheet. Should this cause any problem?
Part Number: ISO7341-Q1 Other Parts Discussed in Thread: ISO7741 , ISO7710 , ISO6741 Dear team,
Can you please help to share the comparison table of ISO7341FCQDWRQ1 & ISO7710FQDWRQ1? Thank you for your help in advance.
Hi Meng, ISO7341-Q1 specifications include both DC VI conditions in the parameter I showed above. Current consumption is the same in both DC VI conditions for this device. Since Si8641 has a different method to transmit data across the device's isolation…
Part Number: ISO7341-Q1 Dear team,
If the Vin is not equal to the Vout, can the device work normally? For example, Vin=3.3V, Vout=5V.
Thanks & Best Regards,
Sherry
Part Number: ISO7340-Q1 Other Parts Discussed in Thread: TMS320F28379D , ISO7341-Q1 , ISO7342-Q1 Tool/software: Hi Everyone,
In my design I am using ISO7340-Q1 digital Isolator between the TMS320F28379D and motor controller PWM signal. I saw a 300 to…
Hi Arthur,
Thank you for using E2E forums!
ISO732x currently has IBIS models available in the product folder under the Tools and Software tab, the link for the same is here : http://www.ti.com/product/ISO7341-Q1/toolssoftware .
This IBIS model can…
Part Number: ISO6762 Hello,
we were wondering, why the ISO6762 is neither listed in the UL File No. FPPT8.E181974, nor in the UL-CA-L181974-24-32205102-8, even though it is mentioned under "PRODUCTs COVERED" in "USR/CNR - Single Protection, Non-Optical…
Hi Tom,
Please see attached the updated UL certificate. It lists ISOM8111 (DFS package) at 5000 Vrms.
I'll be posting this certificate online within the next month.
Thanks, Saleem Marwat
UL Certificate of Compliance File E181974 Vol 4 Sec 6.p…
Conor,
I will work to get answers on the above, but our systems and product teams are still largely out for the holiday, so it may take some time to run this down.
As far as I am aware. I do not believe we have a published certificate specifically…