Part Number: ISO7421 Tool/software: Hi,
Currently we are using ISO7421 as digital isolator for UART communication.
On both sides supply pins of IC, we have given of switching regulator and IN/OUT pins are connected to controllers.
But currently…
Part Number: ISO7421 Other Parts Discussed in Thread: ISO6421 Hi,
About the ISO7421AQDRQ1 isolator, it's ok to place 3.3V at the input of the isolator while the supply is 0V for a long time? It will not cause aging?
The absolute maximum rating is…
Part Number: ISO7741DBQEVM Tool/software:
Hello,
I am using ISO7741DBQR and ISO7421MDREP in one of our designs. This is a very dense, 20 layer circuit card. The datasheet indicates we need to leave all copper layers below the IC free of copper. This…
Part Number: ISO7421 Other Parts Discussed in Thread: ISOS141-SEP Tool/software: Hi,
Which option is more suitable for a design to be used in space: Hi-Rel Products/Enhanced Products or AEC-Q100 components with similar construction to SEP?
Other Parts Discussed in Thread: ISO7421-EP Tool/software: Is the answer of the related topic also valid for ISO7421-EP?
If not, how should I connect the unused channel?
Part Number: ISO7421E Other Parts Discussed in Thread: ISO7721-Q1 , ISO6721-Q1 , , ISOW7841 , ISOW7741 , SN6505B , ISO7741-Q1 , ISOW7741-Q1 Dear team,
I am looking for the digital isolator of automotive grade with 2.5kv ISOLATION and found this part…
Part Number: ISO7421 Hi Team,
Can you have look at the following customer questions, please?
Can you, as the manufacturer, make a statement on the part of TI as to what extent the high-voltage strength of the ISO7421D / ISO7420D component may be limited…
Part Number: ISO7421 Hi,
I just got a claim from a customer regarding communication problems which is caused by a defect of an ISO7421.
The electronic environment is between -20°C and 25°C (it's truck trailer with built in refrigerator) and is sealed…
Part Number: ISO7421 Other Parts Discussed in Thread: ISO7721 , Hi,
Due to the current market situation I wanted to replace the ISO7421D with an ISO7721.
For power reduction during sleep mode, the Vcc is turned of via a µC-Pin (ATMEGA168-PA) but the…