Part Number: ISO7720 Other Parts Discussed in Thread: PSPICE-FOR-TI , Tool/software: Hello
I could see that Digital galvanic isolator simulation models are either IBIS model or transient SPICE model.
In order to perform analog simulation, I need Spice…
Part Number: ISO7720 HI, TI Q&A Community,
Could you let me know the electrical model of barrier capacitance and resistance of digital isolator such as ISO772x?
Thanks in advance,
YJ
Part Number: ISO7720
Hi TIer,
I would like to discuss the supply current ICC2 for ISO7720.
1. If use 5V supply voltage and supply current Icc2 2.2-3mA, the ISO7720 is internal automatic use data rate 3Mbps? right?
2. Is the propagation delay time spec…
Part Number: ISO7720 Hi Team,
Excuse me, why does the UL of ISO7720 only have Single protection?
According to the TUV certificate, it should be able to satisfy Double. thanks.
Part Number: ISO7720-Q1 Other Parts Discussed in Thread: ISO7720 Hi team,
For ISO7720, it’s descripted 5000V rms isolation rating, it means 5000*1.414 V DC isolation rating, right?
Thanks,
Scarlett
Part Number: ISO7720 Hi Sir,
My customer is looking a 2-ch isolation device for analog signals input(single-end) for AHD/TVI signals, the BW is 30MHz.
May I know if ISO7720 can be used?
If it can't, could you please advise a device to me?
Part Number: ISO7720 My name is Dustin Braico and have a question about the absolute maximum voltage for Vcc. The datasheet shows 6V and im sure that only covers a DC level. Is there any information on how much energy or what level of spikes or ripple…
Part Number: ISO7720 Hi Team,
Looking for IEC60601-1 of CSA Certificates(test report) for the following two part numbers;
ISO7720DR
ISO7721DR
Our costumer need this information.
Could you please let us know if you have any information?
Regards,
Hi…