Hello,
Thank you for your inquiry.
Th PSPICE model is located in the ISO7741-Q1 product page under the Design and Development ---> Design tools & simulation tab: ISO7741-Q1 data sheet, product information and support | TI.com .
This PSPICE model…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7741 Hello,
I'm using ISO7741-Q1 (non-F version) in an automotive project.
From Table 8-2 Functional Table it is clear that the output will be HIGH, when VCCI is "powered down (< 1.7V)" and…
Part Number: ISO7741-Q1 Hi team,
My customer is considering to use this device.
In the datasheet, all of the characteristics are shown in the condition of VCC1=VCC2.
Can the customer use this device in a condition like below?
VCC1=5V
VCC2…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7741 Hallo TI Team,
For internal EMC analyzes, I need the working frequency of the ISO774.
Unfortunately I couldn't find anything about it in the data sheet or on their website.
Could…
Part Number: ADS1018-Q1 Other Parts Discussed in Thread: ISO7741 , ISO7841 , ADS1118-Q1 , , ADS1018 Tool/software: for providing digital isolation I am planning to use ISO7741/ ISO7841 with analog SPI ADC ADS1018IDGST. can you please suggest your opinions…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7741 Hi,
I would like to understand better the criteria for selecting an isolating component for reinforced insulation:
If we take the ISO7741-Q1 component, there is a big discrepancy on…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7741 , Hello E2E,
in the maximum ratings, the output current is limited to +/-15 mA.
Is this value related to a maximum peak output current value or is this an output average / rms…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7741E-Q1 Hi all,
Do we have pin to pin digital isolator with ISO7741-Q1 beside ISO7741E-Q1?
I could not find in the ti.com. Can you help me?
Thank you
Part Number: ISO7741E-Q1 Other Parts Discussed in Thread: ISO7741 , , ISO7741-Q1 , ISO7841 Dear experts, the ISO7741 is rated for reinforced insulation for a maximum of 800V. The internal device parameters would allow a maximum working voltage of 2121V…
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7741 Dear Sir/Madam,
In our custom card we are using ISO7741-Q1 digital isolator for SPI interface signals to other card. One side(Vcc1) we are powering up using 3.3v and other side(Vcc2) we…