Part Number: ISO7742 Other Parts Discussed in Thread: SN74LVC2G34 Dear team,
Customer want to use ISO7742 for signal isolation. But they are not sure if the current of ISO7742 is big enough to driver other signals. As datasheet shows may smaller than…
Part Number: ISO7742 Other Parts Discussed in Thread: ISO1541 , ISO1540 , ISO7241C Dear ,
Can I use ISO7742 to monitor ISO1524 function for i2c isolated ?
Part Number: ISO7742 Other Parts Discussed in Thread: ISO7021 , ISO7041 Hi team,
Just would like to confirm with you that can ISO7742 P2P replace ADUM1442? Do you have any other device recommendations?
Thank you!
Regards,
Ivy
Part Number: ISO7742-Q1 Dears,
ISO7742-Q1 has been applied on 48V PTC heater product.
My end customer(Global Automotive Tier-1) asked me how the below test affects the isolation of ISO7742-Q1.
(the below test : short circuit test of case 1 and case…
Part Number: ISO7742-Q1 Other Parts Discussed in Thread: ISO7742 Dear team,
Could you help to check leakage current for below?
Part. No
Temp. (DC 14V)
Leakage Current
ISO7742QDBQQ1
+ 125 ︒ C
…
Part Number: ISO7742 Hi support team.
My customer has two questions below.
1. Is the ISO7742DWR package dimension and land pattern diagram correct with the understanding of DW0016A on pages 42 and 43 of the data sheet?
2. Is it correct to understand…
Part Number: ISO7742-Q1 Hey Team,
What would the effect be of losing one of the grounds on the ISO7742-Q1 Digital Signal Isolator?
Are they redundant internally?
Best, Dajon McGill