Hi Xing,
Applying an input voltage, that is greater than its respective VCC by 0.5V, violates the absolute maximum rating of the device, as stated in datasheet. Hence, TI doesn't guarantee device operation or reliability of device once a device is subjected…
Part Number: ISO7742-Q1 Other Parts Discussed in Thread: ISO7742 , ISO1212 , ISO1211
Hello TI Team,
Please find the attached schematic of "ISO7742QDWQ1" Digital Isolator and review the same.
Circuit is designed for 2 Digital Input and 2 Digital…
Part Number: ISO7742-Q1 Other Parts Discussed in Thread: ISO7742 , Hi ,
I am using ISO7742 in my project application and I am trying to measure the rise time, fall time and propagation delay of the device under the following operating conditions
Vcc1 =…
Part Number: ISO7742-Q1 Hi,
I'd like to ask you on the issue of EMC RI Test. There is the communication signal disconnection when testing from 1.2GHz to 1.4GHz, and other frequency band is no problem. That point is from 70V/m to 140V/m of 1.2GHz. But…
Part Number: ISO7742-Q1 Hi team ,
I am using ISO7742F in my project application. During validation, I find that the VDDX UVLO threshold values as mentioned in the datasheet is not matching with my results.
I have provided 3.3V to VCC2 and IND on Side…
Part Number: ISO7742-Q1 Other Parts Discussed in Thread: UCC5304 , ISO7762 , , AMC1336 hi, I need to know if the below devices are in LOW voltage mode at the start.
UCC5304
ISO7762
ISO7742-Q1
thank you!
Part Number: BQ79656-Q1 Other Parts Discussed in Thread: ISO7742 If we want to use BQ79656 as a single device, which ISO774X should we use? For example, I want to make a BMS for a 12 s battery. Therefore, I can use one BQ79656. Does ISO774x support Uart…