Part Number: ISO7760-Q1 Tool/software: I want to use ISO7760-Q1 for IO isolation. I want to connect VDD1=VDD2=5V. Can you give me supply dissipation or required maximum supply current of ISO7760-Q1?
Thanks,
Part Number: ISO7760 Other Parts Discussed in Thread: SN74LVC1G07 , SN74LVC07A Tool/software: Hi Team,
Do we have OPEN COLLECTOR output digital isolator, customer need such device with 6 channels & reinforced isolation.
If we don't have, whether we…
Part Number: ISO7760 Tool/software: There's a safety certification in the d/s 6.7, however the E181974 is just able to find the certificate number, but there's no electrical information of certification.
could you help to offer it! thanks.
Part Number: ISO7760 Hello Team,
looking at below table I calculate a max frequency of 1/6ns = 167MHz which means a data rate of max 333Mbps should be possible.
Please let me know if my calculation is correct. My customer plans to use the ISO7760 at…
Part Number: ISO7760-Q1 Other Parts Discussed in Thread: TVS0500 , TPS25947 , Hi,
Please refer to attached drawing
I am designing a MCU board which will communicate with a daughter board to get sensor data.
Some data lines are connected between MCU and daughter…
Hi Rao-san
Thank you for your reply.
I understood the device has been sufficiently tested and verified.
My customer wants to have the proven data that the carrier frequency of ISO7760 is 450MHz.
EMI data of ISO7760 is also ok for him.
Best regards,
Shunsuke…
Part Number: ISO7760 Other Parts Discussed in Thread: ISO7763 HI
Could you help suggestion suitable devices can Replacement ADuM163N0BRZ
Thanks
ADuM160N/ADuM161N/ADuM162N/ADuM163N (Rev. A) (utmel.com)
Part Number: ISO7760 Hello TI experts,
I just saw the part name ISO7760F in ISO7760 datasheet.
but i cannot find any description in it.
what is the difference between these 2 devices?
Best regards,
Chase