Part Number: ISO7760 Dear e2e support,
My customer needs to protect the ISO7760F inputs from high voltages (up to 90V during several seconds), in case of dysfunctions inside his system/application.
So the ISO inputs have been protected by series resistors…
Part Number: ISO7760 Hi Team,
My customer is using the ISO7760F to isolate signals from an FPGA and signal to analog switch.
We’re trying to understand if it’s acceptable to run this part at different Vcc based on each own gnd reference. In the datasheet…
Part Number: ISO7760 Dear Sirs,
My customer asked us about layout for ISO7760.
He is troubled about the layout.
He is thinking of placing ISO 7760 on TOP and Bottom to make good use of the pattern.
Is it possible to place the same ISO 7760 on the bottom…
Part Number: ISO7760 Other Parts Discussed in Thread: TVS0500 , ISO1212 , ISO1211 Hello,
I'm using ISO7760 on an interface card. It is powered by 5V and Its outputs are routed to line connector directly. The line interface is subjected to EN61000-4-5 4kV…
Part Number: ISO7760 Hi team,
How about the output current of each channel when working at 5V and 6-ch are all at normal work?
In the POWER RATINGS part of the datasheet, it seems the maximum current is about 242mW/5.5V=44mA, but in the ABSOLUTE MAXIMUM…
Part Number: ISO7760-Q1 Other Parts Discussed in Thread: ISO7710-Q1
Dear team,
I know ISO7710-Q1 is 1-channel version of ISO7760-Q1.
But ISO7710-Q1 Viowm(Maximum working isolation voltage) DC is 1414V. On the other hand, ISO7760-Q1 has Viowm DC is 2121V…
Part Number: ISO7760 Dear Technical Support Team,
How do I estimate for current consumption of ISO7760?
input output
Case1: 3.3V ⇒ 5V (Vcc1 :3.3V、 Vcc2: 5V)
Case2: 5V ⇒ 3.3V (Vcc1 :5V、 Vcc2: 3.3V)
Datasheet shows Vcc1=Vcc2=5V or 3.3V…
Hi,
I hope your were able to resolve any noise issues you were facing and are able to use ISO7760 in your application. I will go ahead close this E2E thread. If you have more questions, please do create a new post for the same. Thank you.
Regards, …