Part Number: ISO7762-Q1 Tool/software: Dear Team,
I am currently working on a gate driver design using the ISO7762FQDBQQ1 digital isolator . In this design, I am utilizing only four channels of the isolator, while leaving two channels unused. According…
Part Number: ISO7762 Tool/software: Hello,
I wanted to use ISO7762 part to isolate CAN transceiver. I want to interface VCC1 side of this isolator with 3.3V Microcontroller and VCC2 of isolator to 5V CAN transceiver. As per isolator ISO7762 datasheet…
Part Number: ISO7762-Q1 Other Parts Discussed in Thread: ISO7241M , ISO7241C Tool/software: Dear TI experts,
My customer asked about digital isolator which data rate is over 150MHz.
But I think maximum data rate of digital isolator is 100MHz. (in…
Part Number: ISO7762 Hello,
can anybody please explain me how to read the LOT or Date Code marking on the ISO7762 package?
What does "04C4CDT" mean?
Thanks in advance, Niels
Other Parts Discussed in Thread: ISO7762 Hi,
We are using a "ISO7762FDBQR" Digital isolator in an industrial device on SPI and UART signals.
1. What will be the power consumption and dissipation of the isolator at ambient and at +70 deg?
SPI…
Part Number: ISO7762 Other Parts Discussed in Thread: ISO1640 , ISO7742 , TXB0102 , ISOUSB211 Hello Team, We are planning to use the IC ISO7762QDWQ1 for one of our applications. We need to isolate JTAG signals before flashing the MCU. It has a propagation…
Other Parts Discussed in Thread: ISO7762 Tool/software: We are using isolator ISO7762 in a 5 wire SPI bus and need to ensure we can achieve the max data rate 6 Mbps up to 125C. There a number of devices in the path but this IC adds the highest propagation…
Part Number: ISO7762 Other Parts Discussed in Thread: ISO7741 , ISO7761 , CC3220MODA , Hi,
Subjected to the previous Post ADS1018 , We are using Isolators between Energy Meter-ADC IC and Microcontroller (CC3220MODSF12MOBR) as shown in the block diagram…