Part Number: ISO7762 Hello!
Can I use power supply voltage of VCC1 and VCC2 differently in ISO7762? I want to use VCC1 = 5V and VCC2 = 3.3V.
Thank you.
Part Number: ISO7762 Other Parts Discussed in Thread: ISO7840 Hi, a customer is working on a project wihere Viowm 1000VDC(707VAC) with EN61010 reinforced is needed.
ISO7762:
ISO7840:
At the two digital isolators the datasheet refers to EN61010.
Eg. ISO7840…
Part Number: ISO7762
Dear Team,
is it possible to get FIT rates of our digital isolators (in this case the ISO7762)?
The online tool on http://www.ti.com/quality/docs/estimator.tsp does not bring results for this component.
The data sheet mentioned >40…
Part Number: ISO7762 Hi,
Could you let me know how to termination of not using line, please?
For example, at not using B line, I think it is INB=GND and OUTB=Open. Is it correct?
Best regards, Shimizu
Hi Emrys,
Thanks for answer.
Please find attached Skeleton
Here, I have used ISO7762 in multiple slave configuration, But due to output nature of ISO7762--> MISO1 Signal Pulling down due to other ISO7762 and viceversa and we are not getting SPI Slave…
Part Number: ADS131M08 Other Parts Discussed in Thread: ISO7762 , SN74LVC2G125 Hi Team,
I have connected 2 ADC with one MCU as per below configurations.
When we tried to read ADC, only one ADC is reading and other is not?
ADC: ADS131M08
Isolator: ISO…
Part Number: ISO6760 Other Parts Discussed in Thread: ISO7762DWEVM , ISO7760 , ISO7762 Hi TI,
Could you please help me find a replacement for ISO6760FDWR with the same pinout and same package/case.
I have used this in my design and now it is out of stock…
Part Number: ISO7742-Q1 Other Parts Discussed in Thread: UCC5304 , ISO7762 , , AMC1336 hi, I need to know if the below devices are in LOW voltage mode at the start.
UCC5304
ISO7762
ISO7742-Q1
thank you!
Part Number: ISO7740 Other Parts Discussed in Thread: ISO7762 , Hi,
We are currently working on a design that is using ISO7740 and ISO7762 to create a 3kV isolation barrier. The requirement spec we must meet references IEC/EN61000-4-5 (surge) and IEC/EN61000…