Part Number: ISO7763 Hi team,
There is a rather generic question applied to any multi-ch digital isolator - is there any spec defines channel-to-channel isolation voltage? Thanks!
Part Number: ISO7763 During varying steps of a manufacturing process & acceptance testing of a Printed Wiring Assembly, the behavior of an ISO7763FDBQR will permanently change from nominal to a low impedance path from VCC2 (pin 16) to GND2 (pin 9). This…
Hi Jeffrey, The ISO7763 propagation delay (time for a signal to reach from input to output) is typically 12ns and ranges from 6 - 16ns. The propagation delay is expected to be the same in forward and reverse channels as long as Vcc1 and Vcc2 are both…
Part Number: ISO7763-Q1 Other Parts Discussed in Thread: ISO7763 Hi TI-team
My customer trying to use SSOP package for communication between microcomputers in ECU.
Should we consider SOIC as a package that assumes that ESD is applied directly, such as…
Part Number: ISO7763-Q1 Hi TI-team
My customer will use LDO to supply Vcc.
The data sheet recommends 0.1µF capacitance for VCC1 and VCC2.
Is the LDO output capacitor alone not enough ?
Is Vcc still required to have a capacitance of 0.1μF even if…
Part Number: ISO7763 Hello,
I would like to ask if I only use 5 input pins of the IC, is the one not used should be pull-low to GND?
Does this pin can be floating?(Because the IC already has pull-low resistance inside, for example.)
Or if there is any…
Part Number: ISO7763-Q1 Other Parts Discussed in Thread: ISO7041 , ISO7763 Dear TI product management,
we would be very interested in an ultra low power digital isolator like the new ISO7041, but with the following specifications:
- Providing a continuous…
Part Number: ISO7763 Dear All,
our customer would like to use the ISO7763 for isolating a PWM motor control signal.
It is expected to have a signal of some kHz with high and low duty cycle. Will the ISO7763 have any problems with that?
I do not think so…
Part Number: INA239 Other Parts Discussed in Thread: ISO7763 , ISO7741 , INA238 Hi!
I need help with using a low side sensing application with the INA239.
So far I have it working with a high-side sensing application but it does not work for the low side…
Part Number: AMC1311 Other Parts Discussed in Thread: ISO7763 Hi team,
do AMC1311 and ISO7763 these kind of isolated device use different VCC?
ex. VCC1=3.3V, VCC2=5V