Part Number: ISO7820LL
Hi
Need your help to recommend, two-way transmission, with isolation, without EN PIN, can replace the ADN4650 LVDS; The search found that ISO7820LL seems to be more suitable, but our CPU does not enable the trigger signal, and the…
Part Number: ISO7820LL Hi,
I use ISO7820LL to transmit LVDS signal. But i met a question on GND.
Please refer below schematic,
If 3(the VCC1 GND of ISO7820LL) is connection for VCC1, OUTA+ and OUTA-(FP_SYNC_P, FP_SYNC_N) is no output.
If 3(the VCC1 GND…
Part Number: ISO7820LL Hi team,
1. For ISO7820LL, can I/O use AC coupling?
2. If not, can I use DC bias on pin and use ac couple to transmit signal?
3. Which is better, DC couple and AC couple for signal Integrity?
Thanks
Part Number: TIDM-02006 Other Parts Discussed in Thread: ISO7820LL , TMDSFSIADAPEVM , ISO7763 Hi Team, Taking a cue from the TIDM-02006 design guide, our customer has these questions: - In daisy chain FSI, are digital isolators (example: ISO7820LL) like signal…
Part Number: DS90LV804 Other Parts Discussed in Thread: ISO7820LL I wanted to know how many mA the Tx of this component (DS90LV804) has?
Also is there such component (with the same drive strength) and offers data isolation?
Hi Archie,
Thanks for reaching out.
ISO7820 is for isolating CMOS logic signals while ISO7820LL can be used for isolating LVDS signals. Please do share ISO7820LL part with customer and let us know if they have any questions, thanks.
Regards, Koteshwar…
Hi,
Thank you for sharing the waveform, appreciate it. I see that the data signal that is applied 100Mbps which is the max that ISO7820LL supports. To support this datarate, sufficient care has to be taken to keep the test setup and the input clean.
Please…
Hi HY,
I am not sure if you are referring to ISO7820 digital isolator or ISO7820LL LVDS isolator in your post. If you are referring to ISO7820LL, it supports 100Mbps of datarate while ISO7821LLS supports 150Mbps. These are the recommend LVDS isolators…