Part Number: ISO7821LL HI,
When I use ISO7821LL to isolate LVDS signal,I want to consult some questions,
there are some points you can attention in my device:
1.Ethernet cable and RJ45 are used to connect my two devices.
2.LVDS signals are transmited through…
Part Number: ISO7821LLS hello team,
we are looking for and isolation for our project which has mipi csi2 and we came to know that ISO7821LLS has an data rate of 125 Mbps But we need minimum of 900 Mbps data rate. can you suggest any other ic for this…
Part Number: ISO7821LLS Other Parts Discussed in Thread: ISO7821LL , Hi Team,
our customer is looking for isolator for MIPI CSI-2 interface due to safety concern, they find ADN4654 can support MIPI CSI-2 isolator. do you have similar devices? or we can…
Part Number: ISO7821LL Hello,
Does ISO7821LL support DC signal isolation? Datasheet describes that the signaling rate range is 0~100Mbps, but our customer tested that ISO7821LL didn't support DC isolation, while other signaling rate like 6.5Mbps could…
Part Number: ISO7821LL Hi,
The A/D converter is affected by AC main 60Hz noise from RJ45 connector, so there might be another way of using ISO7821LL (with ultra-low isolation capacitance 0.7pF) between LAN Magnetics and MSP432E401 PHY. Is there any concern…
Part Number: ISO7821LLS Other Parts Discussed in Thread: ISO7821LL Hello,
I would like you to confirm about below.
* I would like to make sure detail of Distortion correction function which have ISO7821LLS.
From viewpoint of block diagram, I understood…
Hi Rebecca,
Thanks for reaching out.
MIPI interface is primarily a differential interface hence, ISO6720 cannot be used for MIPI interface directly. We currently do not have isolators that can isolate MIPI interface without needing additional devices…
Part Number: DS90UB913Q-Q1 Other Parts Discussed in Thread: ISO7821LLS Does TI have any SerDes chips which will comply with EN60601 medical standards?
I'd like to know if there are any SerDes chips that are medical grade? or example, is the DS90UB913 medical…
Hi Aaron,
Sorry for the delay in responding. I was checking with the isolation products team (probably should've reassigned this thread to them!).
There is a solution to achieve isolation for half duplex LVDS. It requires more than one device though…