Part Number: ISO7842 Tool/software: Hi TI-Team,
I am looking for information on how the switching characteristics are defined, in particular the specification of the minimum and maximum values. What standard deviation do the minimum and maximum values…
Part Number: ISO7842 Other Parts Discussed in Thread: ISO7742TB-Q1 , ISOW7742-Q1 , ISOW6442 , ISOW7742 Hi: The ISO7842 has a creepage distance in the DWW format of 14.5mm and a Maximum impulse voltage of 9.8kV in air. Is there a matching isolated power…
Part Number: ISO7842 Other Parts Discussed in Thread: ISO7742 Hi Sir,
Current, my project will plan to find bi-directional isolator and support I2C interface, cross review design forum and get this one schematic be reference as picture.
It look…
Part Number: ISO7842 Other Parts Discussed in Thread: ISO6742-Q1 Tool/software: I want to design a gate driver module for a 2.3kv Sic modules. Isolation requirement (reinforced isolation) is given below;
Material Group : 1 Pollution Degree : 2 Altitude…
Part Number: ISO7842 Other Parts Discussed in Thread: STRIKE Tool/software: I plan on using this component to protect the user and circuit board from a lightning strike over a 300 foot cable. Do I need to add TVS diodes to protect the cable side inputs…
Part Number: ISO7842 Other Parts Discussed in Thread: ISO7840 Tool/software: Hello,
according to the datasheet, the maximum allowed value of the output current of ISO7842 is 15 mA. Is it allowed to connect an RC circuit consisting of serially connected…
Part Number: ISO7842 Tool/software: our customer MID Certificate need DTI more than or equal to 1mm,but the datasheet only more than or equal to 21um,if have any report or certificate for this,thanks.
Part Number: ISO7842 Tool/software: Hi Expert,
My customer is using ISO7842DWE package, for pin7, it is not connected in the datasheet, but customer want to connect 3.3V power with 300-500mA continues current.
I am not sure if this pin is high impendence…
Part Number: ISO7842 Other Parts Discussed in Thread: ISO7242C , ISO6742-Q1 , ISO7741-Q1 Tool/software: Hi,
A my account is search for a P2P compatible device with NSi8242W-DSWR which supports TTL input signal. The input voltage threshold of ISO7842…