Part Number: ISOUSB211 Tool/software: We are using the ISOUSB211 in a design. We are only using the ISOUSB211 for the isolation of the DD+ and DD- lines. Therefore, it does not have an isolated power supply and shares the same ground.
The upstream-facing…
Part Number: ISOUSB211 Tool/software: Hello,
We also use the galvanic isolated SN6505 circuit in our ISOUSB211 circuit. It is natural that there is a voltage difference in ISO GND and Digital GND measurements due to the transformer structure. Is it possible…
Part Number: ISOUSB211 Other Parts Discussed in Thread: ISOUSB111
Tool/software:
Hello.
Do you have any plans for a small package for the ISOUSB211 series? I tried to use this product before, but the SSOP (10.30 mm × 7.50 mm) size was too big to fit…
Part Number: ISOUSB211 Tool/software: hi team,
the normal USB can communicate with up tp 1.5 meters. Can this device increase the communication distance? thanks!
Part Number: ISOUSB211 Tool/software: Idea concept
Dear TI
I suggest that the reinforced isolation high-speed mass data transfer capable USB interface developed by TI should be expanded into more sub-products. Using the USB interface, small, high-speed…
Hi Jon,
For full-speed transmissions, the SE0 for EOP width from the transmitter must be between 160ns and 175ns and the waveform that you have shared seem to meet these requirements. Therefore, this eye-diagram is considered a pass for a repeater. Thanks…
Part Number: ISOUSB211 Tool/software: I hear a whine, whistle or hum in my audio application. Does TI have a device that can isolate the USB port and remove noise?
Hi Willie,
Thank you for following up.
I do not have any update to share with you at this time. We are internally trying to thoroughly test and understand the issue you are facing and once we have an update, I will be able to come back. I currently do…
Part Number: ISOUSB211 Tool/software: Hi,
My customer want to survey 4kV digital isolator for 2.5Gbe LAN and USB 10Gbps, do TI have this kind of solutions?
Thanks and Best regards,
Tiger
Part Number: ISOUSB211 Other Parts Discussed in Thread: ISO7710 , ISO7041 , ISO1640 Hi team ,
We are designing a board with ISOUSB211DPR , The schematics is attached and we would like to get your comments on the design
usbIsolator.pdf