Part Number: ISOUSB211 Dear Support Team,
I have a question on whether we can achieve a Creepage > 8mm for the board on which ISOUSB211 is mounted (NOT ISOUSB211 itself).
1. According to the ISOUSB211 datasheet ( Rev.C, page 7), the Creepage is >8mm…
Hi Lyna,
Thanks for reaching out and considering TI offered solution. Please find my inputs below on your requirement and what we have to offer:
The ISOUSB211 matches all of your requirements except the Isolated Power requirement.
IEC 60601-1…
Part Number: ISOUSB211
Hi,
I am evaluating ISOUSB211DPEVM for USB Audio use where the ISOUSB211DPEVM is inserted in between the path of music streamer USB output (type A) and USB DAC input (type B). Another competing product is ADUM4166. Subjective…
Hi Varun,
1. This is the block diagram of the system. There are 3x usbc ports connected through the isolator chip and 1x USB-A port connected firstly to the hub. The eye diagram taken at the USB A connector is good, there is no end of packet or sync…
Hi Peter,
Thank you for quickly lifting pins 6 and 23, testing and confirming that you still see the issue. Yes, you supply configuration for all 3 inputs and the ones generated look good. I don't see any concerns with the supply connections.
The…