Part Number: ISOW1044 Other Parts Discussed in Thread: , TIDA-010938 Tool/software: Hi,
On the ISOW1044 datasheet (page 36), there's a PCB layout example illustrating the recommended placement and routing of external components. We've noticed that the…
Part Number: ISOW1044 Tool/software: In this design, there are 2 ISOW1044 CAN transceivers. The first works as expected, the second functions with regards to CAN reception (haven't tested transmission yet), but exhibits around 215mA of current consumption…
Part Number: ISOW1044 Tool/software: Hello,
I am wondering if it is safe to have VIO powered with 3.3V and Vdd not powered (0V) for this IC for when not in use. Vdd is powered off 5V when in use, but we want to disable the 5V regulator to conserve power…
Part Number: ISOW1044 Tool/software: Hi TI,
Based on space restrictions, I have to place 2x ISOW1044 CAN transceivers on the top and bottom layers directly on top of each other with the circuits physically separated from each other on their own outer…
Part Number: ISOW1044 Other Parts Discussed in Thread: SN6505B-Q1 , ISO1042-Q1 Tool/software: I need a part similar to ISOW1044, CAN transceiver with isolation, integrated power supply and automotive grade.
Part Number: ISOW1044 Other Parts Discussed in Thread: ISOM8710 Tool/software: Dear team
Do we have a device which is similar like ISOW1044, but with a reversed IN(pin2)/OUT(pin14) pin? Currently customer need a isolation CAN with a GPIO from isolation…
Part Number: ISOW1044 Other Parts Discussed in Thread: LMR38010 Tool/software: Hi,
We are facing an issue with ISOW1044 for one of our application. The CAN communication is not happening with VDD 5V and VIO 3.3V. But it works for VDD 3.3V and VIO 3.3V…
Part Number: ISOW1044 Other Parts Discussed in Thread: ISOW1432 Tool/software: Hello,
We are interested in using the ISOW1044DFMR and ISOW1432DFMR isolated CAN / RS422 transceivers in an application where thermal performance is a major driver in the…
Part Number: ISOW1412 Other Parts Discussed in Thread: ISOW1044 , , ISOW7741 Tool/software: Hi,
we are using the ADM2687 in our design and we see "quite some noise" from the chip in TEM cell near field measurement.
For this reason are very interested…