Part Number: ISOW1432 Hi team, Hi Team,
We have a query regarding the ISOW1432 receiver failsafe functionality.We are implementing PBIT (Power-On Built-In Test) and CBIT (Continuous Built-In Test) diagnostics for the RS-485 interface using the ISOW1432…
Part Number: ISOW1432 Dear TI.
I have a question about ISOW1432.
I don't use General purpose logic pin which is IN(14pin) and OUT(7pin).
I'm considering below.
IN(14pin):Connect to GND2 OUT(7pin):Unconnect(Open)
Please let me know if this approach…
Part Number: ISOW1432 Dear TI, I have a few questions regarding the pins of the ISOW1432:
1.Is pin D (pin 2) internally pulled up? In Table 7-1. Pin Functions, there is no mention of an internal pull-up, but in Section 10.8 Device I/O Schematics, it…
Part Number: ISOW1432 Tool/software:
I want to select an isolated RS422 chip with a data rate of 10 Mbps or higher. It doesn't need a separate ISO power supply. The ISOW1432 seems to be a suitable choice. However, there are only two IO pins…
Part Number: ISOW1432 Tool/software: Hi team , Whether RE# should be pulled down or high.I am seeing one of the reference both DE and RE are Pulled down
Part Number: ISOW1432 Can you review this schematic an give me some feedback?
Plesae advise if the connections on the A/B/X/Y pins are correct.
I saw this in the forum and no one poited out tht those connections were wrong:
https://e2e.ti.com…
Part Number: ISOW1432 Other Parts Discussed in Thread: PROFIBUS , ISOW1412 We are considering using the ISOW1432 in Profibus Mode with a data rate of 2.5 Mbps and would like to inquire about its current consumption. Could you please provide information…
Part Number: ISOW1412 Other Parts Discussed in Thread: ISOW1432 , Can ISOW1432 be used instead of ISOW1412 in a design?
Cosidering that ISOW1432 is a faster part, can a capacitor be used between its input/output lines to slow down the device and avoid…
Part Number: ISOW1432 Other Parts Discussed in Thread: ISOW3086 Hi,
We currently have a requirement for full-duplex RS485. Since this chip has two pairs of Tx and Rx, would it be feasible to use it? Thank you.