Part Number: ISOW7742 I have tested my equipment based on ISOW7742FDFMR by IEC 60601-1-2 (class A emissions). The test results showed a very narrow margin from the limits in the 50 to 60 MHz range (graph below, limits for 3m distance from the antenna…
Part Number: ISOW7742 Tool/software: What is the minimum data rate for this component? Can it be used for static signals either high or low for long periods of time?
Part Number: ISOW7742-Q1 Dear TI experts,
My customer test ISOW7742-Q1 in their custom PCB.
During the test, customer found the waveform as below. Could you check it?
Turn off the power supply into Vio during operation
The voltage of Vio (Green…
Part Number: ISOW7742 Other Parts Discussed in Thread: LM2775 , TPS61222 , ISOW7842 Tool/software: Hello:
I would like to know whether ISOW7742 isoltate power supply can be used as an elevetor from an Vdd=3.3V to Visoout=5V, and what is the minumum…
Part Number: ISOW7742 Other Parts Discussed in Thread: ISOW7842 Hello guys,
One of my customers is considering using ISOW7742 instead of ISOW7842.
At this moment, they have a question about ISOW7742 as the follow. Could you please give me your reply…
Part Number: ISOW7742 Other Parts Discussed in Thread: MAX3232E , ISOW7821 , ISO7821 For context, it is a medical device. ISOW7742 is part of an isolated serial port (which includes a MAX3232E). Isolation requirement is 3kVac for 60s. We want the port…
Part Number: ISOW7742 Tool/software: Dear Technical Support Team,
Question about ISOW7742.
7.1 Absolute Maximum Ratings says that the Max value for the EN/FLT pin is Vsi+0.5 (V).
Here, Vsi is defined as input side supply, but for the EN/FLT pin…
Part Number: ISOW7742 Other Parts Discussed in Thread: ISOW7741 , ISOW7741DFMEVM Tool/software: Dear Technical Support Team,
I have a question about decoupling capacitors.
For example , decoupling capacitors for VIO/VISOIN are different between Figure…
Part Number: ISOW7742-Q1 Tool/software: Hi,
I'm working on integrating the ISOW7742-Q1 into a design and would like to have the ability to change the output voltage of the isolated power converter from 3V3 to 5V or vice versa at runtime. What is the…
Part Number: ISOW7842 Other Parts Discussed in Thread: ISOW7742 , Tool/software: Hi Team,
There is the difference between ISOW7842 and ISOW7742 on the input and output waveforms. Please check the attachment and let me know the reason why.
Difference…