Part Number: IWR1443 Hello,
i installed the ccs v12 with mmWave Sensors device support. Here is what i installed: Additionally i installed the mmwave sdk and bios.
Then i tried to import an existing project, but it shows this error:
This project…
Part Number: IWR1443 Tool/software: Dear contact person,
I am try to upload the high accuracy bin in my iwr1443 module and getting issue while flashing.
[ERROR] Cortex_R4_0: !!! Aborting flashing of specified files!!!
Regards,
Abhijeet Si…
Part Number: IWR1443 Tool/software: Dear contact person,
I am using IWR1443 Module and configure it via following commands, but i don't get accuracy on it . Can you please help for configure the module for high accuracy
sensorStop flushCfg dfeDataOutputMode…
Part Number: IWR1443 Tool/software: Dear Person,
I update high accuracy firmware in my IWR1443 Module and i want to read its data but i have little bit confusion that , the data is coming on adc line or in spi line .
Regards,
Abhijeet Singh
Part Number: IWR1443 Hi,
I am looking for the best mmwave sensor to measure depth for an outdoor application. The depths I am looking to measure are from 30 cm to 3 m. I have a FOV of 90degrees, which could be reduced if needed. I need to have a X-Y…
Part Number: IWR1443 Other Parts Discussed in Thread: IWRL1432 , Hi, once customer has written the calibration data to the QSPI flash, the PCB needs a power-cycle to function correctly. Without power-cycle, the IWRL1432 is reading out only 0xFF from the…
Part Number: IWR1443 Other Parts Discussed in Thread: UNIFLASH Tool/software: Dear contact person,
I am try to build iwr1443 high accuracy firmware in code composer studio but not able to build, it shows many errors. Attaching the screen short.
…
Part Number: IWR1443 Other Parts Discussed in Thread: IWR1642 Tool/software: What is the difference between the two radar models, IWR1443 and IWR1642? Can both of these radar models be purchased from TI's official website?
Part Number: IWR1443 Tool/software: Dear contact person,
We are using IwR1443 Module. I want to know about the details of data packet sent by the module. For the configuration of Module we are sending the following command.sensorStop flushCfg dfeDataOutputMode…