Part Number: AWR1843BOOST Other Parts Discussed in Thread: IWR1443 , AWR1843 , DCA1000EVM , IWR1843BOOST , IWR1843 Hi, Happy newyear to everyone! my name is Joo-Hyung Lee and I will perform a FMCW test in a laboratory. I have a question. For mmWave FMCW experiments…
Part Number: IWR1443 Hi,
Is there a way to lower the transmit power during RF init calibration?
I will set TxPowerBackOff to -5dB in profileCfg and perform measurements,
but I would like to keep the calibration transmission power to an output value close…
Part Number: IWR1443 Other Parts Discussed in Thread: TIDEP-0091 I want that the version information is also included in the compiled bin file. We sometimes need to check bin file version later. Please give me advice.
I write version information in main…
Part Number: IWR1443 I have a very simple question.
Am I correct thinking that, if I am capturing complex data from a single receiver channel, then the maximum number of ADC samples I can capture for a single chirp is 4096, ie 16384 (the ADCBuff size)…
Part Number: IWR1443 How do ports A, B, C, D, and pins 0-7 in the GIO register correspond to actual chip pins, such as N4, N7, etc?
If you want to use GPIO_ 0. GPIO_ 1. GPIO_ 2. How should the pin function be configured? Is it achieved through the following…
Part Number: IWR1443 Other Parts Discussed in Thread: DCA1000EVM IWR1443:Using lvds lanes to transmit ADC rawdata
Our project is to use iwr1443 to transmit rawdata to fpga board which isn't DCA1000EVM, we want to develop our own FPGA board. However, i…