Part Number: IWR1642BOOST Other Parts Discussed in Thread: MATHLIB , **** Build of configuration Debug for project vitalSigns_16xx_mss ****
"C:\\ti\\ccs1210\\ccs\\utils\\bin\\gmake" -k -j 8 all -O rm -f C:/Users/ozgur/workspace_v12/vitalSigns_16xx_mss…
Part Number: IWR1642BOOST Other Parts Discussed in Thread: UNIFLASH ******************************************
xWR16xx MMW Demo 02.01.00.04
******************************************
mmwDemo:/>MSS Exception: mss/mss_main.c, line 2111.
Is this error…
Part Number: IWR1642BOOST Hello team,
We're exploring the People Counting example and we would like to get more detailed information on how the detected target velocity (in m/s) and target acceleration (in m/s2) are being calculated. We would like to…
Hi Angie,
Angie Mitchell said: Have you done this testing with something more reflective, like metal?
Yes, they've tried.
Use a large sheet metal to place directly in front of the user, and using the same configuration:
Measurements are taken at…
Part Number: IWR1642BOOST Hi,
I'm trying to measure the diameter of a pipe with the Out of the Box demo. I've configured the board for the highest range resolution (0.039 m) but consistently getting errors in range for the two detected points.…
Part Number: IWR1642BOOST Hi,
Customer tries to use two scripts of matlab: Init_RSTD_Connection.m and RSTD_Interface_Example.m. but never succeed
1. Automation.lua cannot be run using powershell, the page prompts as follows:
2.When using matlab to run…
Part Number: IWR1642BOOST Hi! I have a development board and need help with connecting an external FPGA through SPI lines, I am missing information on the SPI format and the register map.
Do you have instructions on how to extract data through SPI lines…
Part Number: IWR1642BOOST Hi,
On below like TI has provided the RF exposure report for IWER1843BOOST, my customer would like to get the same report for IWR1642BOOST, would u pls help check and share here if have?Thanks.
https://dev.ti.com/tirex/explore…
Part Number: IWR1642BOOST Hi,
I'm trying to develop an application by adding the out of box application to CCS. I am sending the initialization values without using CLI interface.
The resume button is not enabled. Can I learn what caused this?
…
Part Number: IWR1642BOOST Hi,
We are using the IWR1642BOOST device, but have some problem to run debug mode. We flashed "xwr16xx_ccsdebug.bin" file and switched the SOP control headers but device don't enter debug mode.
How to enter/run…