Part Number: IWR1843 Other Parts Discussed in Thread: UNIFLASH , Hello,
Im having a isssue flashing my chip with uniflash and I get these error messages:
[ERROR] Cortex_R4_0: XXXX Received unexpected data!!!XXXX
[ERROR] Cortex_R4_0: Not able to…
Part Number: IWR1843 Tool/software: Hi team,
My customer is experiencing the following issues, using the mktime output time to output the wrong time:
There are the SDK the customer used:
Part Number: IWR1843 Hello,
I'm using own 3TX & 4RX patch antenna with IWR1843, and it works by TDM-MIMO.
I'm trying to narrow the Directivity of patch antenna by mounting a dielectric lens on top of 3TX patch anttena .
This dielectric lens tilts…
Part Number: IWR1843 Hi Experts, We want to enhance the vertical field of view of the device to atleast the total of 50 degrees (+- 25). We are happy with the existing horizontal field of view that is 120 degrees (+-60) As per the specifications of the…
Part Number: IWR1843 Buongiorno,
sono Paola Russo di BlueThink Spa, azienda di consulenza di ingegneria con sede a Milano. Stiamo collaborando con un importante cliente nel settore metallurgico e vorrei richiedere supporto per avere maggiori informazioni…
Part Number: IWR1843 Hi There,
We are using IWR1843 to detect liquid level distance. We are doing some RF cetificate for this device. During the test, we are informed by the cerfication org: Non-compliance. They find a spurious waveform at 28.8Ghz band…
Part Number: IWR1843 Tool/software: When I use the IWR1843, I find that the RF of the chip cannot be started at low temperature, and the simulation error code is: 125U:TX power run time calibration was requested but boot time calibration was not performed…
Part Number: IWR1843 Hello,
I have some questions about your "Range Bias and Rx Channel Gain/Phase Measurement and Compensation".
1) It is indicated that "1. Set a strong target like corner reflector" on the doc. Which is preferable to use: flat plate…
Part Number: IWR1843 Hello,
I'm studying MRR(Medium Range Radar) demo of Radar Toolbox3.30.00.06 using IWR1843. Do you have any documentation of MRR Visualizer? I want to know more about "Record & Replay options".
Please advise. Regards,
Shoko
Part Number: IWR1843 Hello,
When adjusting the transmission power of manufactured radars, we use the following method for adjustment. Once the transmission power adjustment is complete, we save the Self-Calibration results and load them during field…