Part Number: IWR1843 Other Parts Discussed in Thread: IWR6843 , IWRL6432 Hi, I am working on a device that will be attached to the back of a person and I want to detect approaching objects such as people or cars coming behind me while walking around. Since…
Part Number: IWR1843 Other Parts Discussed in Thread: , IWR1642BOOST
We are starting a board spin with the IWR1843 and a 77GHz antenna. We are currently in the process of deciding which specific 77GHz antenna we are going to base our design off. We have…
Part Number: IWR1843 Hello,
I'm studying IWR1843 and I would like to change TX power by <txOutPower> of profileCfg of cfg file.
It is indicated "Transmitter Output power = 12dBm(max.)" IWR1843's datasheet.
1) If I set Transmitter…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: UNIFLASH Hello,
I fail to flash the demo image, and UNIFLASH shows the following error:
I have confirmed:
* SOP[2:0]==101;
* CAN-SPI mode switch: SPI mode;
I don't know what mistakes I have…
Part Number: IWR1843 Hello,
I'm studying IWR1843, and I have some question about "txOutPower", "hpf cornerFreq" and "rxGain" of profileCfg on cfg file.
1) "txOutPower"
I understand how to change TX output power…
Other Parts Discussed in Thread: IWR1843 Hello TI team,
I am currently conducting research on vital sign detection using the IWR-1843 radar. I am interested in implementing a real-time system. I have read several references mentioning that we can obtain…
Part Number: IWR1843 Hello
I'm studying IWR1843. I have a question about the Configration command. I want to use only one of 3 TX antennas and one of 4 RX antennas of IWR1843.
Can I achieve the above configuration using Configration command?
Please…
Part Number: IWR1843 Dear Sir,
I only want to obtain the original data of ADC, so I don't need the participation of DSS. Can we obtain adc data use MSS only? Do you have any relevant examples or ideas?
Best.
Part Number: IWR1843BOOST Other Parts Discussed in Thread: AWR1843 As we apply the following profile configure
profileCfg 0 77.15 7 6 23 0 0 7 1 210 12500 0 1 40
chirpCfg 0 0 0 0 0 0 0 7
The CE EN302264 certification will be fail at Out-of-band as the…
Part Number: IWR1843 Hi Team,
Consumer wants to beamforming the IWR1843 radar. The image currently burned is xwr18xx_mmw_demo.bin They want to change the txPhaseShifter in the .cfg file by modifying it to implement the beamforming straight ahead and display…