Part Number: IWR1843BOOST Tool/software: OS Distribution: Ubunutu 22.04
ROS2 Distribution: Humble
I have installed ROS2 humble to run ros2 ti mmwave_ti_ros packages to see point cloud data. Previously, I checked with ros1 with bionic 18.04, which works…
Part Number: IWR1843BOOST Tool/software: Using the ROS driver to get a point cloud and display it in rviz, what determines the colour of the different points of the point cloud? How can I read these specific values without going through DCA1000?
Part Number: IWR1843BOOST Tool/software: Dear Ti support team,
Hope you are doing well.
I am writing to ask some questions about mmWave radar(I am using IWR1843BOOST).
Since the changing of phase is very sensitive to small movement, like vibration, …
Part Number: IWR1843BOOST Other Parts Discussed in Thread: UNIFLASH , IWR1843 , IWR6843ISK , IWRL6432 , IWR1642 , IWRL6432BOOST Tool/software: Hi,
Iam Working with IWR 1843 BOOST mmwave fmcw radar.. i need help in the objectives iam working with..
1.) i want…
Part Number: IWR1843BOOST Tool/software: Im using IWRL1843boost for traffic monitoring,
how can I make the .cfg load on board boot automatically?
is the "Hard code config" applied to this board?
which .cfg is recoomand? I found there are 2…
Part Number: IWR1843BOOST Hi,
I succeeded to setup and connect the EVB IWR1843Boost with my PC with the TI dev cloud.
What is the right way to:
1. Set Real and Imaginary data for each Tx channel from the EVB?
2. Record into my PC the Real and Imaginary…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWR1443BOOST Tool/software: dear Sir
I have opened the communication port on my PC as shown below and am communicating, but midway through, data stops being sent from the IWR1443BOOST.
Recieving…
Part Number: IWR1843BOOST Tool/software: IWR1843BOOST can't get point cloud via ti_mmwave_rospkg under ubuntu system when there is no problem with wiring and power supply.
Part Number: DCA1000EVM Other Parts Discussed in Thread: IWR1843 Tool/software: Dear Ti support team,
Hope you are doing well.
I am currently using mmwave studio CLI to get the raw data from IWR1843 and DCA1000
I am wondering how can I trigger the data…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWR1843 Tool/software: Hello, I would like to ask if the initial phase of the baseband signal of TI's IWR1843 is fixed. My current scenario is: there are two IWR1843s that need to transmit and…