Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWR1843 Tool/software: Hello, I would like to ask if the initial phase of the baseband signal of TI's IWR1843 is fixed. My current scenario is: there are two IWR1843s that need to transmit and…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: DCA1000EVM , Tool/software: Hi,
I can use the UART on the IWR1843BOOST to acquire point cloud data, or use the DCA1000EVM to acquire raw data through LVDS.
Currently, I want to use LVDS to…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWR1843 Tool/software: I would like to use IWR1843 to get the information of the object's motion velocity as well as its reflection RCS information without using additional DCA evaluation module…
Part Number: IWR1843BOOST Hi, thank you for the previous support.
I try to connect the EVB with the software "mmwave_studio_02_01_01_00_win32".
We have a problem connecting to the EVB, which connected to COM port 5:
I try to connect with thw…
Part Number: IWR1843BOOST Tool/software: After the project compiled, I noticed that it only generated a C674x_linker.cmd file, while the MRR demo project includes an additional dss_mrr_linker.cmd file. It seems that dss_mrr_linker.cmd is related to memory…
Alan,
The hw interrupt should be generated based on adcbuf configuration and the same signal is exposed to both MSS and DSS.
Alan Milne said: I've had a look through MAIN and the INIT parts of both, and there's nothing obvious, but it may be that there…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWRL1432BOOST , IWR6843 , AWR1642BOOST Hello!
Hope everyone is having a great week. I am just getting started with the mmWave radar labs and examples and was wondering which lab within the existing…
Part Number: IWR1843BOOST I'm facing a software crash issue with our radar system in the MRR lab. Here's the breakdown:
FPS Dependency: As discussed in this thread the radar's frame rate (FPS) depends on the SUBFRAME_MRR_PERIODICITY_VAL parameter…
Part Number: IWR1843BOOST Other Parts Discussed in Thread: IWR1443BOOST Dear Sir
I received the following answer to my question.
This is already working with mmwave Demo Visualizer running in function mode.
What I would like to know is that I sent the…