Part Number: IWR6443 Tool/software: TI C/C++ Compiler Dear TI
The newest toolbox have the fall detection py file how to use it ?
We need re build it ? and where can find the related documents ?
BR
Part Number: IWR6443
Hi,
In the bootmode - SPI section of IWR6843 Bootloader Flow :
Follow the communication protocol used by the mmWaveSDK mmWaveLinkrlDeviceFileDownload API (described in the mmWaveLink API Doxygen documentation referenced in the mmWave…
IWR6843 & IWR6443 are Production Ready!
Single-chip 60-GHz to 64-GHz intelligent mmWave sensor production device now available.
(Non-Functional Safety Devices)
____________________________________________________________________________________…
Part Number: IWR6843 Other Parts Discussed in Thread: IWR6443 , SYSBIOS Hi,
For IWR6443/6843 R4F, I cannot find the HWI interrupt priority and latency information in sysbios (bios_6_83_02_07\packages\ti\sysbios\family\arm\v7r\vim), can u help share similar…
1. Yes, you can use the interface in picture 1 to get 1D/2D FFT results using mmWave Studio.
2. It is the device datasheeet.
IWR6843, IWR6443 Single-Chip 60- to 64-GHz mmWave Sensor datasheet (Rev. E) (ti.com) - section 8.10.11
AWR6443, AWR6843 Single-Chip…
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/933401/compiler-iwr6443-second-boot-loader-question
This solves the problem but then SBL_METAIMAGE_OFFSET + my updated meta-image size overlaps with the back-up image.
Any idea what options…
Hi Hsincheng,
Yes, this refers to the energy level of each range bin.
Please see this thread for more info on the format: https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1166296/iwr6443-q-format-of-range-profile-and-noise-profile/4389967…
Hi Alec,
It's not a HW issue. HW is connect to 6443 customized board.
Uniflash select IWR6843, and use IWR6443 BIN, then it works, flash succeed, and succeed runs.
Uniflash select IWR6443, and use IWR6443 BIN, then it failed. Uniflash error! image…
Other Parts Discussed in Thread: IWR6443 , IWR6843 , MMWAVEICBOOST , IWR6843ISK Hi team,
I would like to buy IWR6843 or IWR6443 model, which is 60GHz radar. I would like to develop my own solution for traffic monitoring using these radar. In order to do development…
Hi Rivrat,
In terms of latency, this is what the user guide mentions:
Specifically to the devices, here are some tables that indicate the capabilities:
IWR1642 || IWR6843 (i.e. DSP version)
IWR1443 || IWR6443 (i.e. HWA version)
The HWA version of the…