Part Number: IWR6843 Other Parts Discussed in Thread: IWR1843 , , , IWR1843BOOST , Hi,
My customer tests Industrial toolbox 4.3.2 for people counting on IWR6843ISK-ODS EVM board, and wants to migrate such code onto her own IWR1843 PCB. Does TI provide…
Part Number: IWR6843ISK Other Parts Discussed in Thread: MMWAVEICBOOST , ,
Champs,
When reviewing the board design files of IWR6843ISK, Carrier Board (MMWAVEICBOOST) and IWR6843-ODS, 60-pin HD connectors show difference direction.
[1] IWR6843ISK…
Koichiro-san,
You could refer the IWR6843ISK If the design is targeted RO4835LOPRO based substrate material.
In the below design file (Developed in Altium) has complete information with all the geometry for the Package to PCB transition and as well…
Hi,
Jonathan Jones2 said: Can you let me know the maximum transmit power of the IWR6843 under fault conditions.
The maximum output power of the IWR6843 is 10dBm as stated in the datasheet, this should be the max under all conditions. if you implement…
Part Number: IWR1642BOOST Other Parts Discussed in Thread: IWR1642 , UNIFLASH Hi everyone,
I'm trying to reuse the existing project in labs under industrial toolbox (4.11), i followed step by step indications on how to use the 3D people counting on…
Dear Kim,
Please refer to IWR6843ISK-ODS EVM design. This design uses RO3003 reference PCB stack-up information at 60 GHz.
Thanks and regards,
CHETHAN KUMAR Y.B.
Thanks for your reply. I have 2 more questions about the development kits and hope you won't mind to help:-
- I am thinking to get IWR6843AOPEVM for fall detection application cause it has integrated antenna. I found this example experiment and it is…
Part Number: IWR6843AOPEVM Other Parts Discussed in Thread: IWR6843 Hello,
I would like to use I2C to send data to another device. In this case, the IWR6843AOPEVM is the slave and the other device is the master. Basically the master wants to read a…
Hi Zigang,
My IWR6843ISK-ODS is of version ES2 and I use 02.01.00.00 version of mmWave Studio. The firmware has the following path and the versions are reported back:
ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\radarss…
Part Number: IWR6843ISK Hi Experts,
We have been working with a few of the mmWave sensors (including the IWR6843ISK, IWR6843ISK-ODS and IWR6843AOP-EVM). So far our current approach is to flash the device with the Area Scanner Demo and then use a python…