Part Number: IWR6843ISK-ODS Other Parts Discussed in Thread: IWR6843 , UNIFLASH hello,
Is there any tool(with source code provided) which can running on micro device or linux platform to update iwr6843 firmware
because we may connect a another micro…
Hello Taka-san,
Above picture is in Japanese, hence couldn't understand it, But following your description, it appears that USB to UART drivers of the CP2105 chipset has not been installed.
You need to install the Virtual com port (VCP) drivers please…
Hi Matusan,
Changing the number of chirps from 256 (i.e. 128 x 2) to 32 (i.e. 16 x 2) will reduce the gesture recognition performance and we have not evaluated whether/how it will perform. The gesture demo is provided as-is as a proof of concept but…
Part Number: IWR6843 I have asked the same question before, but it is 'resolved' without resolution, so I will ask it again here. e2e.ti.com/.../3823832
In the following link, it says that relative power is based on the "value".
e2e.ti.com/..…
Part Number: IWR6843 Other Parts Discussed in Thread: MMWAVEICBOOST I would like to try and step through the MMWave Demo using TI-CCS but I am having trouble finding the correct project to load into TI-CCS and then building it.
1. I found some .projectspec…
Hello,
AWR family of devices are for Automotive applications and IWR family of devices for non-automotive, industrial and consumer electronics applications.
Broadly you would review following pages to know more about this:
For automotive applications…
Part Number: IWR6843 Hello,
We are trying to figure out the choice between 2 boards - IWR6843ISK and IWR6843ISK-ODS. Our applications is people tracking while it's mounted on a wall with operation range ~6-7 meters.
The ODS board is designed for a…
Oren golan,
IWR6843 EVM comes with two boards RF board 1)IWR6843ISK and IWR6843ISK-ODS 2) Carrier board (MMWAVEICBOOST). RF board is hosted on MMWAVEICBOOST board. RF board to carrier board interface is lower frequency interface there is no interface…
Hello
Would you please let us know if you were able to following the Uart SBL steps which are part of mmwave SDK.
We may be able to help you with more details on the Nov- 16th.
In the mean time please see if these threads help you :
https:/…
Hi Connor,
Apologies for late reply.
We tried multiple experiments with advanced profile configurations for out-of-the-box demo application. During our experiments, we are not able to detect multiple objects when one object is behind other, But if…