Part Number: IWRL6432AOP Hi,
I am designing a custom PCBA based on IWRL6432AOP for human presence detection up to X meters away.
My idea is that the board will have a single 4-pin connector: DC power input (e.g., 12V) and CAN bus (CAN_H/CAN_L). I…
Part Number: IWRL6432AOP We need to have a lens to reduce beamwidth and increase gain
for the devie IWRL6432AOP,
How we have to mount the lens on the device,
We have a circular PCB holding the device on topside,
Please share the fixing and mounting…
Part Number: IWRL6432AOP Other Parts Discussed in Thread: IWRL6432 Hi TI team,
I want to flash my mmwave radar sensor using JTAG connector (10 pin). Can you please tell which debugger i need to flash and also provide the flashing guide?
Part Number: IWRL6432AOP Hello,
We are working on radar FCC pre-compliance testing for IWRL6432AOP chipset and need your support. Could you please share:
Recommended radar configuration tool
Configuration commands for test/continuous…
Part Number: IWRL6432AOP When i am Disconnecting the RADAR_1V2 and RADAR_1V8 the sensor generating the 1.2V at RADAR_1V8 why it is like that?
I using power optimize mode with 3.3V, 1.2V and 1.8V
Part Number: IWRL6432AOP Hello TI Team,
We are designing a custom board based on the IWRL6432AOP device.
Our design includes an EMI shield can, and we need to route four connections from inside the shielded area to the outside:
VCC
GND…
Part Number: IWRL6432AOP Hello,
My customer is experiencing large spikes in battery voltage and temperature using the device. Can you please fill me in on the maximum current draw seen from a IWRL6432AOP device? (this is not an evm, this is a production…
Part Number: IWRL6432AOP Hi team,
Recently i had tested the IWRL6432AOP for people tracking using ceil mounting configuration "Tracking_3Persons_AOP_9_feet_ceiling_mount_v4_AOP" as per the user guide where it able to detect the moving person infront…
Part Number: IWRL6432AOP
Hi Team, we are designing a custom board based on IWRL6432AOP. I want to confirm, Can programming/flashing and Debugging of IWRL6432AOP be done only through the JTAG interface terminal on the PCB and an External Debugger from…
Part Number: IWRL6432AOP Hi,
We are designing the new mmWave module based on L6432AOP.
According to the statement on page 33 of the attached document "Parameter Tuning and Customization Guide for the xWRLx432 Motion/Presence Detection Demo," For tracking…