Part Number: IWRL6432AOPEVM Other Parts Discussed in Thread: IWRL6432AOP , IWRL6432 Tool/software: Hi,
I would like to connect IWRL6432AOP board to the online Demo visualizer, but I cannot connect data port successfully, it's like waiting for the…
Part Number: IWRL6432AOPEVM Tool/software: Hi Team,
I installed MM-WAVE_L_SDK_05_05_03_00 on Ubuntu 22.04, but the Visualizer tool did not install. Does it support Ubuntu 22.04? How can I fix this?
Thanks, Rahul chauhan.
Part Number: IWRL6432AOPEVM Other Parts Discussed in Thread: IWRL6432AOP Tool/software: hi there,
we made some tests here with the iwrl6432aop evm. we mounted it on a post at ca. 8m directly downfacing to the ground.
we used the motion and presence…
Part Number: IWRL6432AOPEVM Tool/software: The FTDI USB isn't recognized as a COM port.
The FTDI driver is installed, but It's listed as an unknown device.
Power is being supplied.
D3, D5, and D6 are lit.
D10 is off.
What should I do?
Part Number: IWRL6432AOPEVM Tool/software: Dear Sir/Madam,
I download MMWAVESDK05.05.30 for my board IWRL6432AOPEVM, but when I follow the video to the step of "open the visualizer", it opens then flash out immediately, can you help me solve this…
Part Number: IWRL6432AOPEVM Other Parts Discussed in Thread: SYSCONFIG , UNIFLASH Tool/software: Hello,
I am trying to modify example motion_and_presence_detection_demo_xwrL64xx-aop_m4fss0-0_freertos_ti-arm-clang for IWRL6432AOPEVM board to make it…
Part Number: IWRL6432AOPEVM Tool/software: Hi
Is an external XDS110 debug probe required for debugging via CCS?
Also, is the xds110 compatible with CCS v20?
Thanks
Part Number: IWRL6432AOPEVM Tool/software: Hi,
is it possible to break off the sensor part of IWRL6432AOPEVM and still use it by connecting a 12-pin cable between J8 and J9?
This would allow more flexible placement of the sensor for evaluation.
…
Part Number: IWRL6432AOPEVM Other Parts Discussed in Thread: UNIFLASH , IWRL6432 ,
Tool/software:
Hello!
I am exploring the 6432AOP and running some of the pre-built images and the visualizers, while a bit quirky, does work eventually. I have been…
Part Number: IWRL6432AOPEVM Tool/software: I used the demo, Motion and Presence Detection. In that Configuration,
I need Ceiling Mount, to capture the human location data. I need to enable the human/non-human classifier and also i need minor motion…