Hi,
Masaki Soga said: JESD251 and JESD216D, refer to Section 4.3.8.
Yes, the boot mode configurations mentioned in the section supports only specific protocols.
Regards, Parth
Hi David ,
David Hirst said: Is ti-processor-sdk-linux-j7200-evm-08_04_00_06/board-support/linux-5.10.120+gitAUTOINC+95b90aa828-g95b90aa828/patches the correct place to put the patch prior to doing a build ?
If your question is will it automatically get…
Part Number: J7200XSOMXEVM
I have the a Quad Port Eth expander on my EVM board, when I connect any of the four ports to an ethernet switch I do not see any Link or activity indication. It seems that these interfaces are not configure. How do I enable them…
Part Number: DRA821U Other Parts Discussed in Thread: J7200XSOMXEVM , DRA821 , J721EXCPXEVM question
J7200XSOMXEVM cannot boot with OSPI. Please let me know the SW settings, tiboot3.bin, tifs.bin, and OSPI PHY Pattern files that can boot OSPI.
usage env…
Part Number: J7200XSOMXEVM Other Parts Discussed in Thread: DRA829 , DRA821 Hello,
I am trying to set the can interface up, bit I am receiving the message that "can" is unknown device.
Furthermore, I checked the dtb file from the sdk: 1. Overview…