I have the F28335 experimenters kit and I was using CCSv3.3 when I ran into the error in "Failed Software Reset". After reading the various related posts in this thread and others, I thought I would briefly explain my experience as it has not been described…
Hi Alan,
Please see below output of OFD command:
OBJECT FILE: MULTI_GCU_CORE2_v0.1.out
Object File Information
File Name: MULTI_GCU_CORE2_v0.1.out
Format: TI-COFF Version 2 …
Hello,
Here are some files tinyxmlparser.asm.txt linker.map.txt
lnk.txt
Building target: "ST4539XL_release_EVM_core0.out"
Invoking: C6000 Linker
"C:/MOP/TEXAS/c6000_8.3.12/bin/cl6x" --cmd_file="C:\depot\salamandre_int/TransceiverResource/Projects…
Hi,
I don't think the issue with with the section marked PROGBITS or not. I was trying to get map for the elf image generated for another example for A72.
See udma_memcpy_testapp_mcu1_0_release_readelf.txt
Can you help me understand what are you trying…
Hi Brijesh Jadav,
I have changed the link file of mcu2_1 as you said before. Move the origin of MAIN_MSRAM_0 to 0x70100000 in the file.
I want to know what is special about the address 0x70100000, why we need to offset the address here?
I tried to generate…
Part Number: DRA829V Hello Team,
We are using 1GB LPDDR4 DRAM from ISSI - IS46LQ32256EA-062B2LA3, where while doing the DDR stress test we are seeing that the Walking 0s is failing continuously. This pattern we are observing in multiple iterations. We…
Hello Ki,
Thanks for looking into the issue.
Attaching two files.
build file --> build.txt
output file --> project_zero_CC26X2R1_LAUNCHXL_tirtos_ccs.out
Regards,
Pothirajan.K
/cfs-file/__key/communityserver-discussions-components-files/81/4087…
Hi Venkat,
I've attached my "audioSample.out" app from the following application.
Also, attach your binary so that I will try at my end.
C:\ti\pspdrivers_01_30_00_06\packages\ti\pspiom\examples\evm6747\audio\bin\iDebug
audioSample.txt
Hi Yordan,
Just want to let you know this is an urgent issue from end-customer and we can show you the real waveform and video directly to you by email too.
Elaborate everything for all again:
Customer found Ti5718's GPIO got gitter issue when IPU update…